The CryptoAuth Trust Manager kit has been developed to work with the Kudelski IoT SaaS to offer PKI service and in-field provisioning. The board contains the ECC608-TMNGTLS Trust Manager device which is a pre-provisioned variant of the ECC608. The ECC608-TMNGTLS device will work in combination with the keySTREAMTM Software-as-a-Service (SaaS) powered by Kudelski IoT. The device comes pre-provisioned with a set of cryptographic keys to connect to keySTREAM SaaS. When deployed in the market place, the IoT device containing the ECC608-TMNGTLS will connect to the keySTREAM SaaS which will give ownership of the IoT device to the intended owner by provisioning the device "in-field" with its custom PKI, symmetric keys and/or data.
Open your keySTREAMTM account using this link: https://mc.obp.iot.kudelski.com/products/iot
The CryptoAuth Trust Manager kit consists of the ECC608-TMNGTLS, ATSAMD21E18A as the main MCU., an onboard debugger and a user defined switch and used defined LEDs. The main MCU comes pre-programmed with Microchip`s Security and Computing Group (SCG) kit protocol. This protocol takes care of the communication between the CryptoAuthentication devices and the host MCU over the USB HID interface. Data transfers between the secure authentication IC and the host MCU is indicated by the Status LED.
A wide variety of other Microchip devices can be used in conjunction with the EV10E69A board including the ECC204, ECC206, SHA104, SHA105, SHA106, TA010, TA100 and TA101 by inserting the appropriate mikroBUS board into the mikroBUS header of the DM320118.
The package consists of CryptoAuth Trust Manager Development Board.
|
Title
|
Date
|
||
|---|---|---|---|
| CryptoAuthLib | 01 Jan 1970 | Link |
Additional mikroBUS Hardware Tools