We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Microchip Launches New LoRa® Module Designed for North American Low-Power Wide-Area Networks (LPWAN)

New RN2903 Wireless Modem is FCC Certified for Use in the 915 MHz Band


CHANDLER, Ariz., Feb 29, 2016 — Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced an addition to its LoRa® technology product line. The new RN2903 wireless modem works with North American Low-Power Wide-Area Networks (LPWAN) and is FCC certified for use in the 915 MHz band. The RN2903 modem is designed to be an efficient way to add long-range LoRaWAN™ network capability to any embedded design by integrating a proven LoRaWAN protocol stack running on a low-power PIC® microcontroller, along with the LoRa radio and embedded antenna matching circuit.

Driven by the LoRa Alliance, LoRa technology is able to achieve a range of up to 10 miles and 10-year battery life. The technology targets low data rates and low-duty-cycle applications such as energy metering, location tracking, utility infrastructure monitoring and control, smart city and agriculture. Although predominantly used for the uplink of sensor data, bidirectional communications allow real-time acknowledgement of mission-critical data and downlink control of remote actuator nodes.

“LoRaWAN is already the dominant LPWAN technology choice in Europe, with numerous private and public network deployments,” said Steve Caldwell, vice president of Microchip’s Wireless Solutions Group. “Until today, the rollout of LoRaWAN in the USA has been hampered only by the lack of credible end-node solutions – which the cost-optimized RN2903 from Microchip solves. Microchip was the first to pass LoRa Alliance certification and we plan to continue to be an innovator in this space and a proud member of the LoRa Alliance.”

The RN2903 is designed to be easy to adopt, which minimizes research and development investment and speeds time to market. The simple ASCII-over-UART interface can be controlled by any embedded system, even down to a tiny, eight-pin PIC12 MCU, and the embedded antenna matching circuits and FCC modular certification require minimal radio expertise.

For more information about RN2903, visit http://www.microchip.com/RN2903-022916b

Pricing and Availability

The RN2903 is fully available now, priced at $10.90 each in 1,000-unit quantities. ‘Mote’ development boards (part number DM164139) are also available for purchase, priced at $69.99 each. For additional information, contact any Microchip sales representative or visit Microchip’s Web site at: http://www.microchip.com/RN2903-022916b.

Follow Microchip:

Note: The Microchip name and logo, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries.  PICtail is a trademarks of Microchip Technology Inc. in the U.S.A. and other countries.  All other trademarks mentioned herein are the property of their respective companies.

About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Technology website.

Editorial Contact:
Cathy Gedvilas
(480) 792-4386

Chelsey Kruger
(480) 792-5047
 
Brian Thorsen
(480) 792-7182
Reader Inquiries:

1-888-624-7435

Microchip Technology