Need Help?

Privacy Policy

Live Chat

Designing and Deploying 5G Network Infrastructure


Wireless connectivity is expanding into autonomous vehicles, virtual and augmented reality, smart homes, smart cities, smart factories and other markets. Many of these leading-edge applications are based on networks made up of sensors and other devices that connect to the Internet of Things (IoT). Next-generation 5G wireless networks offer the extended capacity, performance and features that these connectivity applications require. We provide products with advanced features and technologies for creating and deploying 5G wireless equipment and network infrastructure. 

Interactive 5G Network Diagram


Next-Generation Requirements for 5G Network Infrastructure


5G technology has been developed to provide some key improvements over 4G LTE wireless infrastructure, including:

  • Offering up to 10 times more bandwidth for mobile high-speed Internet access
  • Offering up to 10 times more connections for IoT and sensor devices
  • Reducing network latency by up to 10 times

5G uses a variety of frequencies to deliver the high bandwidth and low latency that next-generation mobile broadband connectivity requires. On the lower end, it continues to use LTE frequencies of < 2.5 GHz. However, it has been expanded to support 3.5 GHz and, in some cases, it may support up to 6 GHz. Many carriers are planning to implement 5G connectivity at classic microwave (28 GHz and 32 GHz) frequencies and at V band and E band millimeter wave (up to 71 GHz) frequencies to provide even more bandwidth at higher speeds.

5G Radio Access Networks (RANs) incorporate macrocells and small cells to create Heterogeneous Networks (HetNets) that can further enhance performance and boost capacity.

To support 5G mobile networks, telecommunications carriers around the world also need to upgrade their wired access, backhaul and core networks. Our solutions can be used macro base stations, small cells, and microwave backhaul, midhaul and fronthaul and RAN transport equipment.

Blog Posts About 5G Network Infrastructure


Taking the Brakes Off O-RAN Deployment

This blog post considers what can be done to accelerate the uptake of O-RAN infrastructure.

Minimizing Cost and Time to Market for O-RAN Hardware

This blog post takes a look at the technologies and support that semiconductor manufacturers can provide for rapid and cost-effective development of Open Radio Access Network hardware.

Do I Really Need GNSS Timing Receivers in Every 5G Aggregation Site?

5G wireless communication networks require very tight time synchronization at every node to maximize spectrum usage efficiency and capacity throughput.

Microchip Technology Embraces Open Innovation: A Journey With O-RAN Alliance

Discover the details of our journey with the O-RAN Alliance, including the steps we took to join, the driving forces behind our engagement and the extensive benefits that extend across Microchip Technology.

Product Categories for 5G Network Infrastructure