Low-Power, Zero-Drift, Ultra-High-Precision Op Amps for the Most Critical Applications


Our zero-drift operational amplifier (op amp) portfolio utilizes input offset voltage correction to minimize offset related errors. These self-correcting op amps provide the highest level of DC performance, even in the harshest environments. Some of the features of these op amps include:

  • Industry-leading performance with maximum offsets as low as 2 µV
  • Offset drift as low as 15 nV/°C, which enables accuracy across temperature extremes
  • Additional electromagnetic filtering on select devices provides extra protection in electrically harsh environments

Zero-Drift Op Amp Products


Related Articles 


amplifiers ic

How Do I Eliminate “Flicker Noise” in My Amplifier Design? 

While there are many different sources of noise within an operational amplifier, perhaps the most mysterious and frustrating noise source is what is known as flicker noise. How does one deal with this dominating, low frequency noise? If 1/f noise is a big concern, then selecting a zero-drift amplifier is the best solution.

zero-drift op amps

Zero-Drift Amplifiers: Taking the Good With the Bad

The use of zero-drift amplifiers continues to grow due to the superior dc precision that these devices offer. However, there is a downside to this performance – time domain limitations.  

op amps

The Tried-and-True Operational Amplifier (Op Amp): An Overview

Operational amplifiers are still an integral component of most electronic systems. Given the ubiquitous nature of the op amp, let us take a step back and review the elements of an operational amplifier and why it is still so useful in today’s electronics.

op amp

Why Is Op Amp Start-Up Time Important and How Do I Measure It?

This article will discuss the differences between op-amp start-up time vs. settling time and slew rate. We will also walk through a case study for measuring start-up time.

Are You Working on an Automotive Application? 


The low-power and low-noise performance of our AEC-Q100-qualified amplifiers and comparators makes them excellent choices for automotive designs.

automotive op amps

Amp'titudes Episode 1 - Amplifier Bandwidth and Slew Rate

In this premiere episode of Amp-titudes, we will provide a brief look at the slew rate specification for operational amplifiers, and how this specification applies to an amplifiers performance.