This course is a one-day training course that builds on the concepts introduced in the Introduction to PolarFire FPGAs training class. This class focuses on using the I/Os of PolarFire FPGAs to implement high-speed serial interfaces and source-synchronous designs. We will facilitate hands-on lab exercises using the PolarFire FPGA Evaluation Kit to provide practical applications of the material presented.
This class is held at Microchip's facility located on North First Street in San Jose, CA. Students who are unable to travel to San Jose can attend remotely via the web.