Title |
Title
A CAN Physical Layer Discussion
|
---|---|
Name |
Name
AN228
|
Date |
Date
06/24/2015
|
Application Categories |
Application Categories
Automotive /
Network Systems - CAN
Peripheral /
CAN
|
Description |
Description
Many network protocols are described using the seven layer Open System Interconnection (OSI) model, as shown in Figure 1. The Controller Area Network (CAN) protocol defines the Data Link Layer and part of thePhysical Layer in the OSI model. The remaining physical layer (and all of the higher layers) are not defined by the CAN specification. These other layers can either be defined by the system designer, or they can be implemented using existing non-proprietary Higher Layer Protocols (HLPs) and physical layers.
|