We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Single Pair Ethernet (SPE) 10BASE-T1S and 100BASE-T1 Devices Transform IIoT at the Edge and in Higher-Speed Applications

Microchip’s SPE offering reduces cost and complexity of IIoT edge devices while supporting higher-speed Ethernet-everywhere architectures and applications 


CHANDLER, Ariz., March 7, 2023 — SPE technology is setting the stage for all-Ethernet IIoT and industrial Operational Technology (OT) networks that are built with a new class of synchronized low-speed Ethernet edge devices and a simplified cabling infrastructure for latency-sensitive traffic streams. Microchip Technology Inc. (Nasdaq: MCHP) today announces new industrial-grade SPE products that will help fulfill SPE’s promise, from 10BASE-T1S MAC-PHYs that more easily connect edge IIoT devices to the cloud, to industrial versions of its 100BASE-T1 Time Sensitive Networking (TSN) Ethernet PHY transceivers and switches that enable higher-speed applications across far-reaching Ethernet networks.

“Microchip is helping to fuel the adoption of zonal architectures in industrial applications with our new MAC-PHYs that connect to many of Microchip’s microcontrollers (MCUs) to reduce the design complexity and implementation costs for bringing a host of sensors, actuators and other products into the new 10BASE-T1S network infrastructure,” said Matthias Kaestner, vice president at Microchip. “With these new 10BASE-T1S MAC-PHYs and industrial versions of our 100BASE-T1 TSN products, we are making it easier to connect the physical world to the cloud while enabling a seamless Ethernet architecture throughout the IIoT and other industrial networks.”

Microchip’s new LAN8650 and LAN8651 10BASE-T1S MAC-PHY Ethernet Controllers with Serial Peripheral Interface (SPI) simplify the implementation of zonal architectures by enabling basic MCUs, rather than higher-level MCUs with a Media Access Controller (MAC), to be used when creating sensors, actuators and other devices for the edge of OT and IT networks. These low-speed devices do not need their own communication system, and Microchip’s MAC-PHYs connect them into a standard Ethernet system all the way to the cloud over simple twisted-pair wiring.

For industrial applications that require higher bandwidth, designers can use MCUs with an integrated Ethernet MAC. Microchip now offers an industrial-grade version of its LAN8770 100BASE-T1 Ethernet PHY Transceiver that provides 100 Mbps transmit and receive capability over a single Unshielded Twisted Pair (UTP) cable.

Microchip’s SPE portfolio is enhanced with industrial-grade versions of its LAN937x and LAN938x Gigabit Ethernet TSN Switches with integrated 100BASE-T1 PHYs. These scalable, secure and compact SPE switches include hardware time-stamping features for supporting IEEE 802.1AS (gPTP) and IEEE 1588v2 (PTP) time synchronization, among other TSN functionality. Energy-efficiency features include ultra-deep-sleep power down with remote wake for battery applications.

“Microchip’s industrial-grade 100BASE-T1 offerings reduce cost, wiring and installation complexity by enabling a complete SPE network from device to server,” said Charles Forni, vice president of Microchip’s USB and networking business unit. “Our industrial-grade SPE offerings are built to withstand harsh environmental conditions across an expanded temperature range while delivering enhanced performance, such as safety, security and extended cable reach, to support industrial applications.”

Development Tools

To support the design efforts of these new products a set of network analysis tools and evaluation boards are available including the LAN8651 EVB and EVB-LAN9383. Microchip’s MPLAB® Harmony v3 provides software support to configure, debug and program designs, while the MPLAB Network Creator provides a quick and intuitive graphical interface for switch configuration.

Pricing and Availability

Microchip’s LAN8650 and LAN8651 10BASE-T1S MAC-PHYs and its LAN937x and LAN938x 100BASE-T1 Ethernet Switches and LAN8770 100BASE-T1 Ethernet PHY are available for purchase at Microchip’s Purchasing and Client Services website, www.microchipDIRECT.com.

For additional information or to purchase, contact a Microchip sales representative or authorized worldwide distributor.

Resources

High-res images available through Flickr or editorial contact (feel free to publish):

About Microchip

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

                                                                                          ###

Note: The Microchip name and logo, the Microchip logo and MPLAB are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Editorial Contact:

Kim Dutton
480-792-4386
kim.dutton@microchip.com

Reader Inquiries:

1-888-624-7435