We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Radiation-Tolerant (RT) PolarFire® FPGA Achieves MIL-STD-883 Class B Qualification, Paving the Way for Power-Saving, High-Speed Processing in Space

This major step toward QML Class Q and Class V spaceflight qualification enables system integration using Microchip’s RT PolarFire® FPGAs, leveraging their power and radiation advantages over SRAM-based FPGA alternatives. 


CHANDLER, Ariz., Aug. 16, 2022—Spaceflight system developers often commit to designing with new components only after they have received MIL-STD-883 Class B qualification and are in the process of meeting the Qualified Manufacturers List (QML) Class Q and Class V standards for spaceflight component reliability. Microchip Technology Inc. (Nasdaq: MCHP) has now achieved the first qualification milestone with its RT PolarFire FPGA, enabling designers to begin assembling spaceflight systems that take advantage of this FPGA's superior computing and connectivity throughput and its significantly lower power consumption and immunity to configuration Single Event Upsets (SEUs) compared to SRAM-based FPGAs.

“Microchip is a QML-certified manufacturer of high-reliability FPGAs for space applications and has attained the highest available Class V qualification multiple times on FPGAs and other integrated circuits,” said Shakeel Peera, vice president of marketing for Microchip’s FPGA business unit. “This MIL-STD-883 class B qualification is yet another big step toward solving some of spaceflight’s most difficult system challenges, including reducing satellite signal processing congestion with much lower power consumption and greater reliability than is possible using alternative FPGA solutions. We have started the final step of qualifying our RT PolarFire FPGAs to both QML Class Q and Class V requirements.”

To achieve MIL-STD-883 Class B qualification, RT PolarFire FPGAs passed a series of environmental tests to determine resistance to the harmful effects of natural elements, the conditions of defense and space operations and mechanical and electrical tests. Passing these tests paves the way for QML Class Q and V qualification while demonstrating the reliability advantages of RT PolarFire FPGAs in space. Their embedded configuration switches have been shown to be robust to more than 100 krad of total ionizing dose radiation exposure, which makes them suitable for most earth-orbiting satellites and many deep space missions. Unlike alternative solutions, these FPGAs do not exhibit any configuration upsets in radiation and therefore require no mitigation, reducing engineering expenses and bill of materials costs.

About the RT PolarFire FPGA Family

The RT PolarFire FPGA family brings Microchip’s 60 years of spaceflight heritage to a product line that delivers the necessary computing and connectivity throughput for modern space missions. These FPGAs consume up to 50 percent less power than SRAM-based alternatives while enabling on-orbit data processing systems to meet demanding performance requirements and reliable operation without excessive heat generation in the harsh radiation environment of space. Their unique combination of Logic Elements (LEs), embedded SRAM, DSP blocks and 12.7 Gbps transceiver lanes enables higher resolution for passive and active imaging, more channels and finer channel resolution for multi-spectral and hyper-spectral imaging and more precise scientific measurements using noisy data from remote sources.

The RT PolarFire FPGAs can also be paired with one or more complementary Microchip solutions in today’s spaceflight systems, including its Ethernet PHY VSC8541RT, CAN interface USB-to-UART PHYs, clocks and oscillators from the company’s clock and timing solutions group and power solutions from its analog power and interface group.

Availability

The Microchip RT PolarFire FPGA with MIL-STD-883 Class B screening is available now in production quantities in hermetically sealed ceramic packages with land grid and solder column termination options. Manufacturers who have already adopted these FPGAs for their next-generation spaceflight systems will have their orders scheduled for shipment. Manufacturers who are waiting for successful qualification can now commit to RT PolarFire FPGAs by starting design work. Designs based on these FPGAs are developed and programmed using version 2021.3 of Microchip’s Libero® SoC Design Suite and are supported by development boards and radiation data. Complete information about the Microchip RT PolarFire FPGA family is available on our website.

Resources:

 

About Microchip

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

                                                                                                ###

Note: The Microchip name and logo, the Microchip logo, Libero and PolarFire are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks are the property of their respective companies

 

Editorial Contact:

Brian Thorsen 
480-792-7182
brian.thorsen@microchip.com

Reader Inquiries:

1-888-624-7435