Rollout of Microchip’s MOST50 Networking Devices for Infotainment Systems Continues With New Lexus GS Deployment

Lexus’ Premium Surround Sound Audio System Enabled by MOST50 INICs for Transporting Video, Audio, Packet and Control Data throughout the Vehicle


CHANDLER, Ariz., September 12, 2016 — Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced that its MOST50 Intelligent Network Interface Controllers (INICs) are powering the infotainment systems of Toyota Motor Corporation’s new Lexus GS line of luxury sedans. The new GS line is the latest Toyota brand to use MOST50 in their infotainment system. The Lexus GS is using Microchip’s OS81092 INIC. The carmaker is one of more than 30 manufacturers to rely on Media Oriented Systems Transport (MOST®) technology to transport video, audio, packet and control data throughout the vehicle. 

“Audio quality is clearly important to Toyota, who promotes the Lexus GS audio system as ‘home-audio-system quality in your home away from home’,” said Dan Termer, vice president of Microchip’s Automotive Information Systems Division. “MOST technology delivers through pure digital audio transmission from source to sink—and does so cost-effectively, allowing simultaneous transmission of audio and control over a single cable.”

Microchip’s MOST technology, used in over 200 car models across the globe, features an electrical Physical Layer (ePHY) that is optimized for use with Unshielded Twisted Pair (UTP) copper wire. The result is a system that can predictably and efficiently transport video, audio, packet and control data without time synchronization protocols, using dedicated channels for minimal processor overhead in the main infotainment control unit. The remote-connection-management and remote-control capabilities of the MOST INICs enable further options including the ability to build slim (processor-less) network nodes.

MOST INICs also provide industry-standard hardware interfaces to processor and peripheral devices for the efficient routing of information, which greatly simplifies module designs. End users can immediately use the vehicle’s infotainment system, due to the MOST INIC’s ultra-fast network startup feature.

The MOST Cooperation standards enable automotive OEMs and their Tier 1 suppliers with a proven and well-supported methodology for defining and implementing high-bandwidth infotainment and Advanced Driver Assistance (ADAS) systems, including a standard physical layer and a robust method for system management and control with superior reliability and Quality of Service (QoS). Using MOST technology also results in reduced weight for easier compliance with environmental regulations.

To facilitate development, MOST technology comes with a complete ecosystem of tools, software and support: tools vendors include OptoLyzer MOCCA family and OptoLyzer Studio, both from K2L; the software stack can be MOST Linux® driver, MOST NetServices or DTCP-Stack; schematics and layout reviews such as MOST Check are available; and, multimedia companion IC products include video encoding, DTCP content protection, I/O expansion and power management.

To learn more about Microchip’s MOST networking products, visit MOST501672                                                                         

Follow Microchip:

Note: The Microchip name and logo, the Microchip logo, and MOST are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Technology website.

Editorial Contact:
Cathy Gedvilas
(480) 792-4386

Chelsey Kruger
(480) 792-5047
 
Brian Thorsen
(480) 792-7182
Reader Inquiries:

1-888-624-7435

Microchip Technology