We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!
Item Qty
Your cart is empty.

Protect Critical Infrastructure Networks with the TimeProvider® 4100 Release 2.3 Grandmaster Timing and Synchronization System

Microchip’s new timing grandmaster enhancements improve deployment flexibility, security and scalability


CHANDLER, Ariz., October 13, 2021 Infrastructure communication networks – 5G mobile, utilities, cable, transportation, defense and data centers – acquire and maintain signals for precise timing from Global Positioning System (GPS) or other worldwide satellite constellations. These networks require redundant backup systems when Global Navigation Satellite System (GNSS) signals are unavailable. The TimeProvider® 4100 Release 2.3 precision timing grandmaster available today from Microchip Technology Inc. (Nasdaq: MCHP) meets this requirement with the industry’s very latest IEEE® 1588 v2.1 2019 security standard for protection of timing systems, while also providing an increased level of deployment flexibility and scalability.

Microchip’s TimeProvider 4100 Release 2.3 grandmaster introduces an ultra-resilient multi-client Precision Time Protocol (PTP) optional license, providing customers with up to three connections to other grandmasters in the operator’s network. This capability can be used as a backup for time and phase input. This new option implements the latest IEEE 1588 2.1 standard majority vote mechanism to select the best input for Assisted Partial Timing Support (APTS) backup protection.

Additionally, TimeProvider 4100 Release 2.3 provides more deployment flexibility with support for two PTP server profiles on every Ethernet port. Customers can now optimize usage of these ports without additional hardware investments. TimeProvider Release 2.3 also allows PTP server, PTP client and in-band management to be used on a single port.

TimeProvider 4100 Release 2.3 provides increased security with support for the latest IEEE 1588 2.1 2019 standard. It includes support for architecture guidance security, which uses redundant communication paths between PTP nodes to detect tampering. It also implements out-of-band management mechanisms for detecting tampering, degradation and failures. This timing grandmaster provides complete support for authentication, authorization and accounting (AAA) as well as two-factor authentication. As a software update, TimeProvider 4100 Release 2.3 is available for new and already-deployed systems. Other features include:

  • PTP enhancements including increased capacity of up to 1,000 network clients, which is required for certain applications such as data centers. 
  • Enhancements to the E1/T1 expansion module with new signals such as composite clock and JCC (Japan CC format), both inputs and outputs, for increased integration with legacy systems.

TimeProvider 4100 Release 2.3 can be managed by Microchip’s TimePictra® Synchronization Management System for full Fault, Configuration, Accounting, Performance and Security (FCAPS). Contact your Microchip salesperson for ordering detail.

Resources:

                                                                                            ###

Note: The Microchip name and logo and the Microchip logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. TimePictra and TimeProvider are registered trademarks of Microchip Technology Incorporated in the U.S.A. All other trademarks mentioned herein are the property of their respective companies.

About Microchip

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

Editorial Contact:

Cathy Gedvilas
480-792-4386
Cathy.Gedvilas@microchip.com

Reader Inquiries:

1-888-624-7435