We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Preserve Legacy Low Pin Count (LPC) Investments with the Industry’s First Commercial eSPI to LPC Bridge

Device allows industrial computing developers to integrate the eSPI standard in existing equipment, minimizing development costs and extending product lifecycles


CHANDLER, Ariz., May 28, 2019 — As the industrial computing industry transitions from Low Pin Count (LPC) to enhanced Serial Peripheral Interface (eSPI) bus technology, developers face high development costs to update existing equipment to the new standard. To allow developers to implement the eSPI standard while preserving large investments in legacy LPC equipment, Microchip Technology Inc. (Nasdaq: MCHP) today announced the industry’s first commercially available eSPI to LPC bridge. The ECE1200 bridge enables developers to implement the eSPI standard in boards with legacy LPC connectors and peripherals, substantially minimizing development costs and risk.

Product longevity is critical in industrial computing equipment applications because of the significant upfront investment required. The ECE1200 eSPI to LPC bridge allows developers to maintain long lifecycles while supporting the eSPI bus technology that is required for new computing applications utilizing the next generation of chipsets and CPUs. To reduce risk for developers, the eSPI bus technology went through intensive validation for industrial computing applications and has been validated with leading processor companies.

“Microchip has been at the forefront of providing eSPI since the standard’s infancy in the computing space,” said Ian Harris, vice president of Microchip’s computing products business unit. “We are continuously bringing new products to market to help the industry transition to eSPI. The ECE1200 extends our leadership in this market and allows customers to implement eSPI without sacrificing years of investments in legacy LPC equipment.”

Designed for today’s eSPI requirements, the ECE1200 detects and supports Modern Standby mode with low standby current. This helps industrial computing developers manage operating costs and efficiencies, while maintaining the features end users expect from modern devices. The ECE1200 is simple to implement and does not require any software.

Development Tools

To streamline development, the ECE1200 comes with a BIOS porting guide, schematics and a layout guide.

Pricing and Availability

The ECE1200-I/LD is available today in a 40-pin VQFN package for $2.66 each in 10,000-unit quantities.

For additional information, contact a Microchip sales representative, authorized worldwide distributor or visit Microchip’s website. To purchase products mentioned here visit our purchasing portal or contact a Microchip authorized distributor.

Note: The Microchip name and logo, and the Microchip logo, are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

About Microchip

Microchip Technology Inc. is a leading semiconductor supplier of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company’s solutions serve more than 125,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

Editorial Contact:
Cathy Gedvilas
(480) 792-4386

Chelsey Kruger
(480) 792-5047
 
Brian Thorsen
(480) 792-7182