We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

New Long-Reaching USB 3.2 Compatible Reclocker/Redriver Devices for Automotive and Industrial Applications

Microchip’s EQCO510 and EQCO5X31 devices offer a solid two-channel solution to send high-speed data signals up to 15 meters in both directions


CHANDLER, Ariz., May 16, 2023 — The standard universal serial bus or USB connection is an industry mainstay that transfers data between two devices. The increase of adding electronic components to applications across the automotive, industrial and consumer industries has spurred the need for far-reaching USB cabling products. To provide long-distance and reliable USB solutions to the market, Microchip Technology (Nasdaq: MCHP) today announces two new reclocker/redriver devices. The automotive EQCO510 and industrial EQCO5X31 reclocker/redriver devices extend USB coverage up to 15 meters for maximum reach and are compatible with the USB 3.2 Generation 1 SuperSpeed protocol.

The EQCO510 and EQCO5X31 are USB reclocker/redriver devices that can send high-speed data signals with a rate of 5 Gbps in both directions. The reclocking feature includes a bit-level Clock-Data Recovery (CDR) that is used to restore signal timing and prevent jitter accumulation. The redriving feature restores the levels and shape of the signal being driven into the next segment such as a cable or printed-circuit board (PCB) trace, thus compensating for signal degradation due to cable attenuation.

“Our customers now have the capability to implement a fast, reliable and long-distance USB connectivity solution of up to 15 meters, extending the three meter standard by five times,” said Matthias Kaestner, corporate vice president of Microchip’s automotive infotainment systems business unit. “These devices also provide our customers with a comprehensive option that reduces board space because of the on-chip clock and small form factor.”

The USB devices are equipped with EyeOpen cable compensation at the receiver to automatically adjust for frequency dependent losses in the cable and adjusting the signal strength between 0 and 24 dB with 1 dB steps. The devices also feature MarginLink signal integrity testing, which allows runtime evaluation of the integrity of the whole signal path.

The EQCO510 and EQCO5X31 ICs support shielded twisted pair and coax cables. The devices include an integrated crystal-less CDR, which reduces the need for additional components and overall board space. Both USB devices are available in a 20-pin, 4 mm QFN package with wettable flanks. The automotive EQCO510 is compliant with automotive reliability standard AEC-Q100 Grade 2 and operates in temperatures ranging from -40°C to 105°C.

Microchip’s USB devices can be used in many automotive applications such as infotainment systems, data communication modules and real-time video systems. Other use cases in industrial applications and consumer products include machine vision, gaming accessories and smart cables.

Development Tools
The EQCO5X31 is supported with two evaluation boards including the EVB-EQCO5X31 USB Type-C® Cable Extender and the EVB-EQCO5X31 USB Type-C Cable Repeater. Both evaluation boards enable the ability to demonstrate use with longer cables.

Pricing and Availability
The automotive EQCO510 is available for $4.82 each in 1,000-unit quantities. The industrial EQCO5X31 is available for $4.38 each in 1,000-unit quantities. For additional information and to purchase, contact a Microchip sales representative, authorized worldwide distributor or visit Microchip’s Purchasing and Client Services website, www.microchipdirect.com.

Resources
High-res images available through Flickr or editorial contact (feel free to publish):

About Microchip

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

###

Note: The Microchip name and logo, the Microchip logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. EyeOpen and MarginLink are trademarks of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Editorial Contact:

Kim Dutton
480-792-4386
kim.dutton@microchip.com

Reader Inquiries:

1-888-624-7435