Microchip Unifies Management of “Terrestrial Time” and “Live-Sky Time” Sources to Enable Resilient Timing for Critical Infrastructure

Company’s TimePictra® 11 timing infrastructure management system works with its BlueSky™ GNSS Firewall to create a unified view for a more secure network timing architecture


CHANDLER, Ariz., June 22, 2021 – Today’s 5G wireless infrastructure has more complex, higher-density synchronization needs than previous-generation networks and is highly dependent on the integrity of “live-sky” timing signals from the Global Navigation Satellite System (GNSS). Microchip Technology Inc. (Nasdaq: MCHP) today announced it has integrated its BlueSky GNSS Firewall with its TimePictra 11 synchronization monitoring and management platform to protect 5G networks and other critical timing infrastructure from Global Positioning System (GPS) signal jamming and spoofing while providing single-console visibility across the entire timing architecture.

“Microchip’s TimePictra system improves overall situational awareness by managing network timing synchronization as well as our GNSS firewall that improves a network’s resilience through real-time GPS threat detection and mitigation,” said Randy Brudzinski, vice president, Frequency and Time Systems business unit. “Our solution’s scalability is particularly valuable for mobile operators who can use TimePictra to monitor GNSS based source clocks along with our secure network-based timing distribution solutions to deploy a highly resilient timing architecture for their transition to 5G.”

In addition to requiring precise timing from GNSS sources, critical infrastructure operators need accurate timing to be distributed across their networks so they can ensure reliable performance and service delivery. TimePictra provides full control and monitoring for resilient timing architectures created with Microchip’s broad product portfolio including its TimeProvider® 4100 grandmasters for 5G network synchronization. It also monitors the health and performance of these networks’ distributed Precision Time Protocol (PTP) client clocks. Integrating BlueSky GNSS Firewall management into the TimePictra console view now gives operators a unified picture of the entire timing architecture and all timing sources.

Beyond supporting 5G deployments, TimePictra enables aviation, railway and maritime ports with a regional, national or global view of GNSS reception. TimePictra in combination with BlueSky GNSS Firewalls monitor key GNSS observables to detect live sky signal anomalies and deliver early alerting so that operators can engage alternate procedures that do not rely on GNSS. These capabilities are increasingly important where public safety is dependent on the position and navigation for daily operations.

Availability

Microchip’s TimePictra timing infrastructure management system with its Blue Sky GNSS Firewall is available today. More information about integrated Clock and Timing  solution.

Resources

High-res images available through Flickr or editorial contact (feel free to publish):

About Microchip

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

                                                                                    ###

Note: The Microchip name and logo, Microchip logo and TimePictra are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. BlueSky is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Editorial Contact:

Cathy Gedvilas 

480-792-4386

Cathy.Gedvilas@microchip.com

Reader Inquiries:

1-888-624-7435