We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Microchip Showcases RISC-V-Based FPGA and Space-Compute Solutions at RISC-V Summit

PolarFire® devices lead in delivering 2X power efficiency, military grade security and highest reliability, which will be extended by the PolarFire 2 FPGA roadmap


CHANDLER, Ariz., December 8, 2022 – Mid-range FPGAs and System-on-Chip (SoC) FPGAs have played a major role in moving computer workloads to the network edge. Microchip Technology (Nasdaq: MCHP) has helped fuel this transition with its award-winning FPGAs, while also delivering the first RISC-V-based FPGAs that provide twice the power efficiency of competing mid-range FPGAs, and feature a best-in-class design, operating system and solutions ecosystem. The company will be showing its solutions at the 2022 RISC-V Summit and previewing its PolarFire 2 FPGA silicon platform and RISC-V-based processor subsystem and software suite roadmap. It will also be discussing a RISC-V-based High-Performance Spaceflight Computing (HPSC) processor that it is developing for NASA and the aerospace and defense industry.

“Microchip was the first to offer FPGAs for power-efficient edge-compute segments, and the first to bring SoC FPGAs into volume production that support the RISC-V open Instruction Set Architecture,” said Shakeel Peera, vice president of marketing for Microchip’s FPGA business unit. “At this year's summit, we are extremely excited to showcase our production ready PolarFire SoC family, partner ecosystem and solutions for today's power sensitive edge compute systems. An added bonus will be a sneak peak of where we are going next to deliver 15X more compute capability to our roadmap." 

The PolarFire FPGA and PolarFire SoC families already deliver the industry’s best thermal and power efficiency in the mid-range segment. Optimized for deploying systems with high compute performance in small form factors, the families have reduced the size and weight of power-constrained systems in applications including industrial imaging, robotics, AI-enabled medical systems and smart defense and aerospace systems. The PolarFire 2 family will go even further up the performance and power-efficiency curve and add new RISC-V-based high-performance compute elements. It also includes a design tool set that takes a new approach to system development, unlocking the full potential of these FPGAs and SoC FPGAs by eliminating the need for smart algorithm developers to understand the intricacies of the underlying FPGA hardware.

Microchip will also be showing its Mi-V solutions ecosystem for supporting RISC-V-based solution stack development. It provides 90%+ coverage for commercial and open-source Operating System (OS) and Real-Time OS (RTOS) packages, and includes other software, middleware and firmware offerings from Microchip and its Mi-V ecosystem partners.

RISC-V Summit attendees can see Microchip’s PolarFire family and Mi-V ecosystem, PolarFire 2 family and design tool suite preview, and HPSC offerings December 13-14, 2022, in Booth #PG5, Hall 2, at the San Jose McEnery Convention Center in San Jose, California. Attendees can learn more about Microchip during the following presentations at the conference:

  • “RISC-V Spotlight: Microchip’s RISC-V Journey to Deliver Innovation from Edge Compute to the Edge of the Solar System,” Bruce Weyer, corporate vice president, FPGA, Microchip, on December 13 in Hall 3 from 11:00 a.m. to 11:10 a.m.
  • “RISC-V Enabling High Performance Spaceflight Computing,” on December 14 in Hall 3 from 9:40 a.m. to 9:55 a.m.   

For complete information about Microchip’s FPGA families click here.

Resources

About Microchip

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

                                                                                          ###

Note: The Microchip name and logo, the Microchip logo and PolarFire are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks are the property of their respective companies.

Editorial Contact:

Brian Thorsen
480-792-7182
brian.thorsen@microchip.com

Reader Inquiries:

1-888-624-7435