We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Microchip’s Low-Power Radiation-Tolerant (RT) PolarFire FPGA is Available in Engineering Silicon and On a Path to Full QML Class V Spaceflight Qualification

Customers can prototype with the same FPGA silicon and package that is now headed for space qualification


CHANDLER, Ariz., Dec. 2, 2020 – Microchip Technology (Nasdaq: MCHP) today announced it is shipping engineering silicon for its RT PolarFire® Field Programmable Gate Array (FPGA) while the device is being qualified to spaceflight component reliability standards. Designers can now create hardware prototypes with all the same electrical and mechanical performance that the space-qualified RT PolarFire FPGAs will provide for high-bandwidth on-orbit processing systems with industry-low power consumption and the ability to withstand radiation effects in space.

“This is a major milestone as we release RT PolarFire FPGA engineering silicon to our customers and begin the spaceflight qualification process through full QML Class V standards,” said Bruce Weyer, vice president of Microchip’s FPGA business unit. “Many of our customers have already jump-started satellite system payload development using our commercial PolarFire MPF500T FPGAs and now all prototyping can be done with silicon that will be identical in form, fit and function to our eventual flight-qualified RT PolarFire FPGAs.”

Microchip is qualifying its RT PolarFire RTPF500T FPGAs to Mil Std 883 Class B, QML Class Q and QML Class V -- the highest qualification and screening standard for monolithic integrated circuits in space. Designed to survive a rocket launch and meet demanding performance needs in space, RT PolarFire FPGAs are ideal for applications including high-resolution passive and active imaging, precision remote scientific measurement, multi-spectral and hyper-spectral imaging, and object detection and recognition using neural networks. These applications require high levels of operating performance and density, low heat dissipation, low power consumption and low system-level costs.

About the RT PolarFire FPGA

Microchip’s RT PolarFire FPGAs increase computational performance so satellite payloads can transmit processed information rather than raw data and make optimal use of limited downlink bandwidth. The devices exceed the performance, logic density and serializer-deserializer (SERDES) bandwidth of any other currently available space-qualified FPGA. They also enable more system complexity than previous FPGAs and withstand Total Ionizing Dose (TID) exposure beyond the 100 kilorads (kRads) typical of most earth-orbiting satellites and many deep-space missions. Their power-efficient architecture reduces power consumption up to 50 percent compared to SRAM FPGAs, leveraging SONOS configuration switches that also eliminate the problem of configuration upsets due to radiation in space.

Availability

The RT PolarFire RTPF500T FPGA engineering models are available in a hermetically sealed ceramic package with land grid, solder ball and solder column termination options. They are supported by development boards, Microchip’s Libero® software tool suite and radiation data. Additional information is available at Radiation-Tolerant Field Programmable Gate Arrays (FPGAs).

Please let us know if you would like to speak to a subject matter expert on Microchip’s RT PolarFire FPGAs and the challenges of high-performance computing in space.

Press image: www.flickr.com/photos/microchiptechnology/48876818616/sizes/l/

About Microchip

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

                                                                                                    ###

Note: The Microchip name and logo, the Microchip logo, PolarFire and Libero are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.