Microchip Enables China to Deploy World's First Bandwidth-on-Demand Services Powered by Optical Transport Network (OTN)

DIGI OTN processors deliver the required technology to enable China Mobile to complete interoperability tests ahead of mass service rollouts


BEIJING, June 12, 2019 /PRNewswire/ -- Carriers in China have been aggressively deploying 100G-capable OTN switching networks over the last few years, and now its largest carrier is poised to launch a new network to support government/enterprise leased-line services that will leverage the international standard for dynamically adjusting OTN connection bandwidth. As the only commercial silicon and software supplier supporting the Hitless Adjustment of ODUflex (HAO) specifications, Microchip Technology Inc. (Nasdaq: MCHP), via its Microsemi subsidiary, provided a benchmark solution based on its DIGI OTN processor family that was key in enabling China Mobile to complete multi-vendor interoperability tests. China Mobile is now able to launch the world's first bandwidth-on-demand leased-line services offering, providing government and enterprise customers the flexibility to adjust their required network bandwidth in real-time as workloads continue to move to the cloud.

Microchip's DIGI family of OTN processors enables carriers to extend OTN from their metro networks to the access layer for use in delivering leased-line and other high-availability and bandwidth-guaranteed services to government, enterprise and data center customers. Each generation of DIGI OTN processors has also integrated HAO functionality so that carriers can provide customers the bandwidth they need when they need it. Without HAO, the bandwidth of the end-to-end connections for delivering these services is fixed, and to change the bandwidth, the connections must be torn down, causing traffic disruption. China Mobile used the DIGI OTN processors to verify technology and software readiness to support roll out bandwidth-on-demand services at scale with the support of multiple system vendors whose OTN equipment demonstrated interoperability.

"China Mobile has deployed bandwidth-on-demand capabilities in our new Government/Enterprise OTN network to benefit from all the advantages of flexible bandwidth and services," said Yunbo Li, project manager at China Mobile Research Institute. "We are the world's first carrier to specify HAO product interoperability requirements and test specifications and now, working with Microchip and our ecosystem of equipment providers, we are pleased to have completed a major step toward large-scale deploying this technology and paving the way for it to become part of our new production network operations."

"We applaud China Mobile as the world's first carrier to complete the necessary interoperability testing to begin a large-scale deployment of bandwidth-on-demand services enabled by flexible OTN switching networks," said Babak Samimi, vice president for Microchip's Communications business unit. "We are proud that our DIGI OTN processors played a pivotal role in proving the readiness of the industry ecosystem, and we believe the momentum behind this technology will now accelerate both in China and around the world, opening a new chapter for carriers to provide an innovative new class of services and new revenue streams tied to their enterprise customers' real-time business demands."

Microchip helped create the HAO specifications, which are defined in the International Telecommunication Union (ITU) G.7044 standard. The company supports this technology through a released Software Development Kit (SDK) for its DIGI-120G, DIGI-G4 and most recent DIGI-G5 OTN processors.

For additional information, contact a Microchip sales representative or visit Microchip's Microsemi subsidiary website.

Resources

High-res images available through Flickr or editorial contact (feel free to publish):

Application image: https://www.flickr.com/photos/microchiptechnology/46954789025

Chip shot: https://www.flickr.com/photos/microchiptechnology/47871196001

White paper: www.microsemi.com/OTN-BOD-WP

About Microchip Technology

Microchip Technology Inc. is a leading semiconductor supplier of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company's solutions serve more than 125,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dep rmation, visit the Microchip website at www.microchip.com.

Note: The Microchip name and logo, the Microchip logo, and Microsemi are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

SOURCE Microchip Technology Inc.

Editorial Contact:
Cathy Gedvilas
(480) 792-4386

Chelsey Kruger
(480) 792-5047
 
Brian Thorsen
(480) 792-7182