We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Microchip Adds Second Development Tool Offering for Designers Using Its Low-Power PolarFire RISC-V SoC FPGA for Embedded Vision Applications at the Edge

Platform extends customer options for designing secure and reliable systems in applications ranging from neural network inferencing to Industrial Internet of Things (IIoT) and factory automation


CHANDLER, Ariz., Nov. 23, 2021 – Microchip Technology (Nasdaq: MCHP) today announced the second development tool offering in its Smart Embedded Vision initiative for designers using its PolarFire® RISC-V System on Chip (SoC) Field Programmable Gate Array (FPGA). The industry’s lowest-power SoC FPGA in its class, the PolarFire device is the only mid-range device of its kind that simultaneously supports dual 4K video processing and quad core RISC-V application-class processors running both the Real Time Operating System (RTOS) and rich operating systems like Linux®

Microchip’s Smart Embedded Vision development platform joins the company’s previously announced VectorBlox™ software development kit (SDK) and IP for using the PolarFire devices to program a trained neural network without prior FPGA expertise. The latest offering simplifies edge-compute solution development in the thermally challenging environments of the IIoT and factory automation applications. The platform’s IP, hardware and tools for these solutions include:

  • Embedded Vision – Supports the following: dual 4K MIPI CSI-2 cameras; HDMI® 2.0 with expansion based on the FPGA Mezzanine Card (FMC); CoaXPress® 2.0; SDI (6 Gbps and 12 Gbps); Universal Serial 10 GE Media Independent Interface (USXGMII) MAC IP with auto-negotiation; and USB 3.1 Gen 1 and Gen 2 protocols.
  • IIoT and factory automation – Enables: Wi-Fi®/Bluetooth®; USB 2.0; SD Card; Embedded MultiMediaCard (eMMC); fully integrated Peripheral Component Interconnect Express (PCIe®) endpoint and root port functionality configured for four lanes; and a mikroBUS™ connector that can be used with Microchip’s Trust&GO platform for secure cloud connectivity.

The platform includes support for Microchip’s Mi-V RISC-V ecosystem including development tools from Green Hills Software and Siemens EDA; commercial RTOS including INTEGRITY®, Nucleus® and VxWorks® ; open-source OS/RTOS such as Yocto and Buildroot Linux, FreeRTOS™, NuttX RTOS and Zephyr® RTOS; and middleware solutions from DornerWorks, Hex-Five Security and Veridify Security.

Microchip’s PolarFire SoC FPGAs combine thermal efficiency, and defense-grade security for smart, connected systems with half the power consumption of alternatives. The PolarFire SoC and the Smart Embedded Vision Platform offer designers the choice of rich operating system-based edge compute, hard real-time, with large 2 MB memory and mixed real-time plus rich OS support. Users can learn one platform and serve three applications.

Availability

Microchip’s Smart Embedded Vision development platform is available now and PolarFire SoC FPGAs are in production. For more information contact FPGA_Marketing@microchip.com.

Press image: www.flickr.com/photos/microchiptechnology/50597292318/sizes/l/

About Microchip

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

                                                                                           ###

Note: The Microchip name and logo, the Microchip logo and PolarFire are registered trademarks of Microchip Technology Inc. in the U.S.A. and other countries. VectorBlox is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Editorial Contact:

Brian Thorsen

480-792-7182

brian.thorsen@microchip.com