We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Accelerate Development of Remote IoT Nodes with the Industry’s Lowest-power LoRa System-in-Package Family

With industry-leading low power consumption, the SAM R34/35 devices enable long-range wireless connectivity while extending system battery life


MUNICH, Germany, November 13, 2018LoRa® (Long Range) technology is extending the reach of the Internet of Things (IoT) by combining long-range wireless connectivity with low-power performance. To accelerate the development of LoRa-based connected solutions, Microchip Technology Inc. (Nasdaq: MCHP) today introduced a highly integrated LoRa System-in-Package (SiP) family with an ultra-low-power 32-bit microcontroller (MCU), sub-GHz RF LoRa transceiver and software stack. The SAM R34/35 SiPs come with certified reference designs and proven interoperability with major LoRaWAN™ gateway and network providers, significantly simplifying the entire development process with hardware, software and support. The devices also provide the industry’s lowest power consumption in sleep modes, offering extended battery life in remote IoT nodes.

Most LoRa end devices remain in sleep mode for extended periods of time, only waking up occasionally to transmit small data packets. Powered by the ultra-low-power SAM L21 Arm® Cortex®-M0+ based MCU, the SAM R34 devices provide sleep modes as low as 790 nA to significantly reduce power consumption and extend battery life in end applications. Highly integrated in a compact 6 x 6 mm package, the SAM R34/35 family is ideal for a broad array of long-range, low-power IoT applications that require small form factor designs and multiple years of battery life.

In addition to ultra-low-power consumption, the simplified development process means developers can accelerate their designs by combining their application code with Microchip’s LoRaWAN stack and quickly prototype with the ATSAMR34-XPRO development board (DM320111), which is supported by the Atmel Studio 7 Software Development Kit (SDK). The development board is certified with the Federal Communications Commission (FCC), Industry Canada (IC) and Radio Equipment Directive (RED), providing developers with the confidence that their designs will meet government requirements across geographies.

LoRa technology is designed to enable low-power applications to communicate over longer ranges than Zigbee®, Wi-Fi® and Bluetooth® using the LoRaWAN open protocol. Ideal for a range of applications such as smart cities, agricultural monitoring and supply chain tracking, LoRaWAN enables the creation of flexible IoT networks that can operate in both urban and rural environments. According to the LoRa Alliance™, the number of LoRaWAN operators has doubled from 40 to 80 over the last 12 months, with more than 100 countries actively developing LoRaWAN networks.

“The LoRa ecosystem is entering a phase of accelerated growth, and as a founding member of the LoRa Alliance, Microchip has been a strong driving force to build the success of this technology,” said Steve Caldwell, vice president of Microchip’s Wireless Solutions business unit. “The SAM R34 continues Microchip’s reputation as a one-stop shop for small, low-power devices that bring the benefits of free software, excellent customer support and dependable supply.”

The SAM R34/35 family is supported by Microchip’s LoRaWAN stack, as well as a certified and proven chip-down package that enables customers to accelerate the design of RF applications with reduced risk. With support for worldwide LoRaWAN operation from 862 to 1020 MHz, developers can use a single part variant across geographies, simplifying the design process and reducing inventory burden. The SAM R34/35 family supports Class A and Class C end devices as well as proprietary point-to-point connections.

Pricing and Availability

Microchip’s SAM R34/35 LoRa family is available in six device variants, providing developers the flexibility to choose the best combination of memory and peripherals for their end application. SAM R34 devices in a 64-lead TFBGA package begin at $3.76 each in 10,000-unit quantities. SAM R35 devices are available without a USB interface starting at $3.66 each in 10,000-unit quantities.

For additional information, contact a Microchip sales representative, authorized worldwide distributor or visit Microchip’s website. To purchase products mentioned here, visit Microchip’s purchasing portal or contact an authorized distributor.

Note: The Microchip name and logo, and the Microchip logo, are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

About Microchip

Microchip Technology Inc. is a leading provider of microcontroller, analog, FPGA, connectivity and power management semiconductors. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company’s solutions serve more than 130,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

Editorial Contact:
Cathy Gedvilas
(480) 792-4386

Chelsey Kruger
(480) 792-5047
 
Brian Thorsen
(480) 792-7182