Functional Safety Certification Packages for Microchip FPGAs Speed Time to Market 

SmartFusion® 2 and IGLOO® 2 FPGAs now add IEC 61508 certification to their Single Event Upset (SEU) mitigation benefits


CHANDLER, Ariz., September 21, 2022—Systems used in many high-reliability commercial aviation, space, defense, automotive and industrial applications require certification to the IEC 61508 Safety Integrity Level (SIL) 3 functional safety specification. To reduce the cost of this process and accelerate time to market for system developers, Microchip Technology (Nasdaq: MCHP) continues to certify its products and tools to industry safety specifications and has now added IEC 61508 SIL 3 certification packages for two more of its System-on-Chip (SoC) FPGA and FPGA families.

“Microchip FPGA families have a broad and historically strong position within the industrial market and are recognized for the high reliability and security of our nonvolatile FPGA technologies,” said Bruce Weyer, corporate vice president of Microchip’s FPGA business unit. “We also have a long history of certifying our products and tools to IEC 61508 SIL 3 and other safety specifications so the end-equipment certification process for our customers is much easier. Adding these packages for our low-power-consumption SmartFusion 2 SoC FPGAs and IGLOO 2 FPGAs is a natural extension for industrial customers who design high-reliability products for the smart grid, automation controllers, process analyzers and other safety-critical applications.” 

Microchip’s safety packages are built on top of the SEU-immune, Flash-based FPGA fabric of the SmartFusion 2 and IGLOO 2 devices, and these FPGAs are certified by independent safety assessor TÜV Rhineland®. Package deliverables include certification of Microchip’s Libero® SoC Design Suite v11.8 Service Pack 4 and associated development tools, plus 28 Intellectual Property (IP) cores, safety manuals, documentation and device data sheets. A safety certificate from TÜV Rhineland is also provided.

Microchip also helps protect customers’ long-term certification investments through practicing customer-driven obsolescence where Microchip commits to build devices used in a certified system as long as customers want to order, and Microchip is able to obtain all sub-elements of a device. This increases confidence that certification will not need to be repeated while also reducing the risk that a part will unexpectedly enter end of life and force redesign or tool flow changes.

About SmartFusion 2 SoC FPGAs and IGLOO 2 FPGAs

Unlike Static Random Access Memory (SRAM)-based FPGAs, Microchip’s Flash-based SmartFusion 2 and IGLOO 2 FPGAs eliminate the need for Triple Module Redundancy (TMR) mitigation that increases total system costs. The SmartFusion 2 SoC FPGA is the only device to integrate an FPGA fabric, Arm® Cortex®-M3 processor and programmable analog circuitry. The low-density IGLOO 2 device consumes up to 50 percent less power than similar devices and is ideal for general-purpose functions requiring more resources than alternative FPGAs can deliver.

Availability

The Microchip safety packages for its SmartFusion 2 and IGLOO 2 devices are available at Microchip’s Purchasing and Client Services website. Complete information about Microchip’s FPGA families is available here.

Resources

About Microchip

Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

                                                                                               ###

Note: The Microchip name and logo, the Microchip logo, IGLOO and Libero are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. SmartFusion is a registered trademark of Microchip Technology Incorporated in the U.S.A. All other trademarks are the property of their respective companies

 

Editorial Contact:

Brian Thorsen
480-792-7182
brian.thorsen@microchip.com

Reader Inquiries:

1-888-624-7435