Microchip PoE Powers Wireless Access Points: Boosting WAP Marketability
Learn more about how Microchip addresses the power and data demands of today’s advanced WAPs.
Power over Ethernet (PoE) has emerged as the go-to solution for powering Wireless Access Points (WAPs), owing to its simplicity and efficiency. PoE not only delivers data to the WAPs via an Ethernet cable but also eliminates the need for a nearby power source. This makes installations more flexible and significantly cuts down on costs, enabling seamless deployment in diverse environments.
Historically, WAPs required data rates of up to 1 Gbps, which was sufficient for older wireless standards. However, with the advent of Wi-Fi 6, the need for much higher data rates—up to 10 Gbps—has become crucial. Wi-Fi 7 pushes these requirements even further, demanding data rates of up to 46 Gbps to fully utilize its groundbreaking features. These advanced wireless standards offer improved connectivity, higher speeds and the ability to support multiple devices simultaneously. They play a crucial role in advancing technologies like ultra-high-definition video streaming, AI-powered applications and the ever-expanding array of connected devices driving the progression of the Internet of Things (IoT).
Microchip has taken a leading role in addressing the power and data demands of today’s advanced WAPs. By redefining wireless connectivity, we aim to deliver greater speed, enhanced data capacity, increased user support and improved efficiency. Our commitment is to address the unique needs of every wireless access point application, ensuring optimal performance and reliability.
We help WAP OEMs offer high-quality, ready-to-use solutions to their customers. By bundling their WAPs with our PoE midspans as powering options, OEMs build competitive advantage and increase sales. They have the advantage of branding it as their own by having their company name and logo at no additional cost. Our PoE midspans empower leading WAP manufacturers with the versatility to offer private-label solutions that are not only compatible with emerging technologies like Wi-Fi 6 and 7 but also support their sustainability goals. Our Green Sustainable (GS) PoE midspans address the rising demand for sustainable technology in line with environmental objectives. If OEMs aim to enhance their WAP offerings and boost sales, leveraging our advanced PoE midspans can be a game-changer.
Microchip's PoE solutions stand out for several reasons:
- Simplify installation and reduce costs
- Offer unparalleled flexibility, supporting data rates up to 10 Gbps
- Leverage single-port indoor and outdoor midspans with desired certifications
- Protect against network threats with advanced cybersecurity
- Enable remote configuration and management
- Prevent unauthorized access with fully sealed and tamperproof systems
- Meet and exceed global energy efficiency standards with GS midspans
By leveraging Microchip’s innovative PoE midspans, OEMs can strengthen their market positioning by offering future-ready solutions to their customers and drive higher revenues. To know more about how our PoE midspans can benefit your business, please visit OEM and Private-Label PoE Systems by Microchip.