We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

The Future of Climate-Friendly Heating and Cooling: Heat Pumps and AC Units

In this post, we explore the benefits of heat pumps and AC units, highlight the market outlook and showcase the innovative solutions that we offer to enhance their efficiency and sustainability.


Introduction

As the world grapples with the pressing issue of climate change, the need for energy-efficient and environmentally friendly technologies has never been more critical. Among these technologies, heat pumps and air conditioning (AC) units stand out for their potential to reduce carbon footprints while maintaining comfort in homes and businesses. Heating and cooling accounts for about half of the global final energy consumption. It is the largest source of energy end use, ahead of electricity (20%) and transport (30%), and is responsible for more than 40% of global energy-related carbon dioxide emissions, according to the International Renewable Energy Agency (IRENA).

In this blog post, we will explore the benefits of heat pumps and AC units, highlight the market outlook according to the International Energy Agency (IEA) and showcase the innovative solutions that we offer to enhance their efficiency and sustainability.

Understanding Heat Pumps and AC Units

Heat pumps and AC units are essential components of modern HVAC (Heating, Ventilation and Air Conditioning) systems. Both are used for regulating indoor temperature using basically the same principle, the refrigerant cycle: evaporation, compression, condensation and expansion.

  • Heat Pumps: These devices transfer heat from one place to another, making them versatile for both heating and cooling. In the winter, they extract heat from the outside air (even in cold temperatures) and transfer it indoors. In the summer, the process is reversed, and heat is extracted from the indoor air and released outside.
  • AC Units: Air conditioners primarily focus on cooling by removing heat from the indoor air and expelling it outside. They are widely used in regions with hot climates to maintain comfortable indoor temperatures.

Heat pump working principle:

Heat pump working principle

Source: Pure Energy Technology Ltd is a registered SEI Supplier of Renewable Energy Solutions to homes and business throughout Ireland.

Why Heat Pumps and AC Units are Good for the Climate

  1. Energy Efficiency: Heat pumps are known for their high energy efficiency. They can deliver three to five times more heating or cooling energy than the electrical energy they consume. This efficiency translates to lower energy consumption and reduced greenhouse gas emissions.

    Two terms are used for rating the efficiency of a heat pump and AC unit;
    • SCOP/Seasonal Coefficient of Performance for heating mode.
    • SEER/Seasonal Energy Efficiency Ratio for cooling mode.

      The higher SCOP or SEER the better efficiency.
  2. Reduced Carbon Footprint: By using electricity instead of fossil fuels for heating, heat pumps significantly reduce carbon emissions. When paired with renewable energy sources, their environmental impact is further minimized.
  3. Versatility: Heat pumps can be used for both heating and cooling, making them a year-round solution. This versatility reduces the need for separate heating and cooling systems, leading to lower material and energy costs.
  4. Improved Air Quality: Modern AC units and heat pumps often come with advanced filtration systems that improve indoor air quality by removing pollutants, allergens and other harmful particles.

Market Outlook: IEA Insights

According to the International Energy Agency (IEA), the global heat pump market is expected to play a crucial role in achieving the United Nations' climate goals. The IEA's Sustainable Development Scenario projects that by 2030, the number of heat pumps installed globally needs to triple to meet the targets set for reducing greenhouse gas emissions. This means increasing the current volume from around 180 million units to approximately 540 million units by 2030.

The IEA also highlights that heat pumps could reduce global CO2 emissions by 500 million tonnes annually by 2030, equivalent to the combined emissions of France and Italy. This significant reduction underscores the importance of accelerating the adoption of heat pump technology worldwide.

The Cold Crunch: AC Units

The IEA also warns of an impending "cold crunch" due to the rapidly increasing demand for air conditioning. By 2050, the number of AC units in use globally is expected to rise to 5.6 billion, up from 1.6 billion today. This surge in demand could lead to a significant increase in energy consumption and greenhouse gas emissions if not managed with energy-efficient technologies.

Demand of AC Units Graph

Microchip Offers Various Solutions for Enhanced Efficiency

Block diagram showing the main components of the outdoor unit for a heat pump

Block diagram showing the main components of the outdoor unit for a heat pump.

Microchip Technology is at the forefront of developing innovative solutions that enhance the performance and efficiency of heat pumps and AC units. Here are some key technologies and reference designs:

  1. Silicon Carbide (SiC) in Power Factor Correction (PFC): SiC technology offers superior efficiency and thermal performance compared to traditional silicon-based components. In PFC circuits, SiC devices help improve power quality and reduce energy losses, leading to more efficient heat pump and AC unit operation. Our 11kW Totem Pole PFC reference design is a prime example, showcasing how SiC technology can achieve high efficiency and compact design in power conversion applications.
    We also have complete SiC Modules. Our mSiC™ MOSFET and diode modules provide flexible options for electrical topology, configuration and materials to maximize your system’s performance.
  2. Inverter Stage: Inverters play a crucial role in regulating the speed of the compressor motor in heat pumps and AC units. Our solutions enable precise control, resulting in optimized energy use and reduced operational costs. We offer IGBT modules in various packages (SP1F, SP3F, SP6C, SP6LI, SP6P and integrated SP6HPD), across multiple technologies (IGBT Trench 3, Trench 4, Trench 4 fast, Trench 5 and the new IGBT Trench 7, or IGBT7) and in various topologies.
    We also offer antiparallel SiC diodes for hybrid SiC versions, providing design flexibility without additional costs.
  3. Auxiliary Power Supply: Reliable auxiliary power supplies are essential for the smooth operation of heat pumps and AC units. We provide robust and efficient power supply solutions that ensure consistent performance and longevity. Our 1000V auxiliary power supply reference design offers high voltage capability and efficiency, making it suitable for a wide range of heat pump and AC unit applications.
  4. Motor Control: Efficient motor control is critical for the performance of heat pumps and AC units. The dsPIC33 Digital Signal Controller (DSC) family is ideal for motor control applications, providing high performance and flexibility.
    Visit our Motor Control Design Center with both HW and SW solutions.
  5. Security: Ensuring the security of heat pumps and AC unit systems is becoming increasingly important as they become more connected. In the EU the newly approved Cyber Resilience Act (CRA) is emphasizing this. Our security solutions, such as the ATECC608A CryptoAuthentication™ device, provide robust security features to protect against cyber threats and ensure the integrity of the system.

Conclusion

Striving towards a more sustainable future, the adoption of energy-efficient technologies like heat pumps and AC units are paramount. These systems not only provide comfort but also contribute significantly to reducing our carbon footprint. With our cutting-edge solutions in SiC technology, inverter stages, auxiliary power supplies, motor control and security, the efficiency and reliability of these systems are further enhanced, paving the way for a greener and more sustainable world.

Call to Action

Are you ready to make the switch to energy-efficient heating and cooling solutions? Explore Microchip's innovative technologies, including the 11kW Totem Pole PFC and 1000V auxiliary power supply reference design, and discover how they can transform your heat pump and AC unit applications for a better tomorrow.

Jesper Andersen, Feb 25, 2025
Tags/Keywords: Sustainability