We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Visit Us at embedded world (ew) 2025

Location: NürnbergMesse, Messezentrum 1, 90471 Nürnberg, Germany

Date: March 11–13, 2025

Stand: 3A-135

Fuel Your Innovation With Us


We’re excited to announce that we will be attending embedded world 2025. Visit us at Stand 3A-135 at NürnbergMesse to explore our latest innovations in industrial and automotive technologies. Discover how our embedded control solutions can fuel your innovation and give you a competitive edge.

Join us for over 20 cutting-edge demos that showcase how our advanced technologies solve real-world challenges. Don’t miss our PIC64 MPU workshop, where you’ll get hands-on experience with the Curiosity PIC64GX1000 Kit and learn to deploy Linux® and Zephyr® RTOS applications.

We’re also hosting multiple speaking sessions at the embedded world Conference, covering topics such as IoT, hardware design and safety innovations. It’s your chance to hear from our experts about the latest trends and advancements in embedded solutions.

Embedded World Demo Preview 


Demo

Description 

10BASE-T1S Extended Reach V2

This demo showcases how to connect 50 nodes over a 98m cable and assemble in a very compact way with a net that helps sustain the cables.

10BASE-T1S Sustainability

This demo showcases how 10BASE-T1S can be used in the sustainability megatrend, enabling the connection of a heat pump with a lean, cloud-based home automation application.

PIC64GX Video and Webserver

Using the PIC64GX Curiosity Kit, this demo highlights a CSI-2® camera input to the video pipeline and output from the pipeline to an HDMI® display while running a web server simultaneously.

PolarFire® FPGAs Enable Edge AI Applications With NVIDIA® Holoscan™

This demo showcases real-time pose estimation—identifying and tracking human body positions and movement. A camera captures a live video, which is sent to the PolarFire FPGA acting as a sensor bridge. Preprocessed data is passed to NVIDIA Holoscan, where advanced algorithms detect and track movements. The final output, displayed on a monitor, includes visual markers highlighting the identified poses.

SLVS-EC™ to Multi-Lane CoaXPress® for High-Bandwidth Video Transmission in Medical Imaging

This demo showcases a PolarFire FPGA processing a 40 Gbps SLVS-EC camera stream and transmitting it over multi-lane CoaXPress to enable high-bandwidth video applications like medical imaging and machine vision.

Automotive Keyless Car Entry

This demo features a keyless car entry system powered by facial recognition. A high-definition video from a camera is transmitted to a PolarFire FPGA using Gigabit Multimedia Serial Link (GMSL), where real-time processing identifies authorized faces and unlocks the car. It showcases the efficiency of GMSL for in-vehicle video transmission and the PolarFire FPGA's capabilities in image processing and machine learning.

Automotive Cockpit

This demo shows the life-size model of a car cockpit with front seats and touchscreens.

On-Cell Foldable OLED with Knob-on-Display™ (KoD™) Technology

Foldable OLED display with a small Knob-on-Display user interface.

Water Fountain Touch Display

A touchscreen tablet is placed under a working water fountain to showcase its waterproof and glove-friendly functionality.

Automotive Interior Lighting

This demo showcases how to use our dsPIC33C DSC to drive multiple mini/micro-LED matrix display modules for automotive applications. The demo features include zonal architecture, high brightness, low power consumption and competitiveness as an alternative to OLED solutions. Graphics are streamed via the 10BASE-T1S Ethernet standard.

Solar Power Management HMI

This solar power management Human-Machine Interface (HMI) graphics demo showcases the capabilities of the SAMA7D65 Curiosity board with a 10-inch 1280 × 800 LVDS display.

Automotive Dashboard GUI with Screen Mirroring

This graphics demo includes an automotive dashboard GUI with screen mirroring of the map from a phone over Wi-Fi® to showcase the capabilities of the SAM9X75 MPU.

Truck Loading Bay Augmented by AI

Discover a parking lot/truck-loading bay monitoring application running on our SAMA7G54, a single-core Arm® Cortex®-A7 based microprocessor. This demo, augmented by AI, leverages Edge Impulse® model creation and training capabilities.

TrustMANAGER Building Access Management

This demo features an electric lock equipped with the EA06V72A development kit that includes an ECC608 TrustMANAGER secure IC. Connected to Kudelski IoT keySTREAM™ SaaS, the demo enables credential rotation and secure access management. While on display, it can 3D-print keys labeled with the Microchip.com/TPDS link, using files stored directly on the printer.

New Concept/Synchronization Solution That Is GNSS Synchronized for Automotive

The Azurite System Synchronizer PLL provides multiple phase-aligned system clocks with a 1 PPS (1 Hz) input clock from GNSS. This enables synchronization of time-of-day information across a vehicle’s Time-Sensitive Network (TSN).

Steering Wheel with Heating and HoD

This demo showcases the lowest-cost implementation of Hands-off Detection (HoD) with combined heating, using a simple low-cost sensor and a single-chip solution with firmware for acquisition and post-processing.

Turnkey Touch Demo

See a demo of the simplicity and new features of our next-generation turnkey touch solution. The demo includes three development kits to explore touch buttons, sensitivity adjustments, wake-up mode testing and the full ecosystem provided.

PCIe® and ASA-ML for Automotive High-Performance Computing (HPC)

Harnessing the power of our latest PCIe switch family and ASA-ML zonal aggregators, this demo enables seamless, multi-host communication, which forms the foundation of a scalable, central compute architecture for automotive HPC.

Smart Warehouse

This demo presents an industrial warehouse solution equipped with energy harvesting capabilities, sensor management, fan control and motor-driven access control. It features a gateway and an HMI designed for industrial applications with a focus on sustainability. The system utilizes wireless technologies, including Wi-Fi, Bluetooth® Low Energy (LE), Thread® and sub-GHz, with the TrustMANAGER demo connected to a 32-bit microprocessor and Ethernet PHY.

Smart Bluetooth Low Energy (LE) Sensor with AI/ML Plus Bluetooth LE Handover Support for Automotive

The demo showcases a toy truck equipped with embedded smart sensors and Bluetooth LE handover support. It highlights how AI/ML-driven smart sensors monitor industrial applications so that goods remain undamaged during transit through features like temperature monitoring, vibration detection and door lock sensors. It also demonstrates Bluetooth LE handover functionality for automotive applications, enabling seamless smartphone access. The demo integrates cutting-edge products, including Bluetooth LE wireless technology, 32-bit microcontrollers, CAN communication and AI/ML capabilities.

AIoT - Agile System Adoption Platform (Industrial)

This demo showcases a complete factory network from sensor to cloud. Discover our AIoT-ASAP industrial demo that features TSN, 10BASE-T1S, 2D touch, advanced network architecture, wireless technologies, graphics and cyber resilience solutions.

 

PIC64 MPU Workshop 


Join our hands-on workshop featuring the Curiosity PIC64GX1000 Kit. Attendees will explore the power of our 64-bit MPU and learn how to:

  • Build and deploy Linux® and Zephyr® RTOS applications
  • Blend traditional OS and RTOS in an amplifier system for real-time tasks
  • Optimize boot times for improved system performance

Learn more about the Curiosity Kit

Conference Speaking Slots 


Date Title Speaker
March 11, 2025
2:15–2:45 p.m.
How Many CPUs Are Too Many? Hugh Breslin
Senior Applications Engineer
March 11, 2025
2:45–3:15 p.m.
Time-Sensitive Networking (TSN) for Industrial Automation Using OPC-UA Martin Kellermann
Marketing Business Development Manager
March 12, 2025
10:00–10:30 a.m.
Moving to RISC-V®: Is It Really That Difficult? Designing Software to Be Futureproof Hugh Breslin
Senior Applications Engineer
March 12, 2025
1:15–1:45 p.m.
How Much Safety Can you “Buy” for Less Than a Dollar? Maria Teresa Jacob
Senior Product Engineer
March 13, 2025
10:30–11:00 a.m.
Seamless Connection Switching in Bluetooth® Low Energy (LE) Applications Gerhard Willbold
Technical Staff Engineer

March 13, 2025

10:30–11:00 a.m.

Why Are 5-Volt Designs Still Relevant? Odd Jostein Svendsli
Business Development Manager
March 13, 2025

10:30–11:00 a.m.

10BASE-T1S: Bringing Ethernet to the Edge for Industrial and Building Automation Mary Sue Haydt
Technical Staff Engineer
March 13, 2025
12:15–12:45 p.m.
Ultra-Low-Power Leak Detect Odd Jostein Svendsli
Business Development Manager

FAQs


Question Answer
Where can I find the embedded world 2025 agenda? You can find the event agenda on the embedded world Europe website.
When does the registration open? Registration is open now.
Where can I buy Microchip products? Visit www.microchipDIRECT.com to buy our products.
What if I have a question? If you have any questions or need assistance, please contact the events team at events@microchip.com