We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest! Update Here
Stay in the loop with the latest from Microchip! Update your profile while you are at it. Update Here
Complete your profile to access more resources.Update Here!

Start with the Most Popular Pre-Configured Use Cases and Use Your Own Credentials


When it comes to IoT security, authentication is one of the foundational concepts that should be implemented first in your design. The trust between the device identity and the cloud platform relies on a chain of trust. AWS IoT supports certificate-based authentication, but the trust in the device identity will depend entirely on how well the device’s private key is protected. If the private key is spoofed, the device can be impersonated by an unauthorized user who can then control the device’s transactions. However, adding authentication presents you with several challenges: securely storing the private key in the device, shipping the private key across the globe for any project and system size and ensuring a secure manufacturing flow. These challenges can be addressed by using the TrustFLEX ATECC608B-TFLXTLS secure element from our Trust Platform family of solutions.

Defining the secure element’s configuration is generally a time-consuming task. The TrustFLEX ATECC608B-TFLXTLS comes pre-configured with the most commonly used use cases to speed up your development and reduce the complexity of the onboarding process. To further simplify onboarding, the device also comes with default generic certificates for thumbprint authentication and overwritable keys. This allows you to either choose the default certificates and keys and lock them afterwards or overwrite the default credentials with your own. When combined with AWS IoT Core Application Program Interfaces (APIs), such as Just-In-Time-Registration and Use Your Own Certificate, you can use a Certificate Authority provider of your choice to create an end-to-end secure authentication. The device’s private keys will have to be provisioned in the secure element using our provisioning infrastructure and the Hardware Secure Modules (HSMs) that are installed in our factories. The key will then be isolated from exposure to software, firmware, manufacturing sites, end users and other third parties. Our ATECC608B-TFLXTLS provides a common criteria JIL “high” rated secure key storage to isolate keys in the nodes. This is especially valuable in TLS networks that are based on a Public Key Infrastructure (PKI) security model and leverage a wide variety of traditional low-power microcontrollers (MCUs).

Ready to Get Started With TrustFLEX and AWS IoT Core?


Step 1: Download the Trust Platform Design Suite, available for Windows® and macOS®, to prototype with your secure element.

Step 2: Buy the development kit of your choice, then prototype and integrate your application code in the microcontroller.

Step 3: Once the C code is working in your embedded application, you are ready to create the configuration file using the TrustFLEX configurator that is available in the Design Suite. After the configuration file is finalized, submit a support ticket to obtain your encryption key. Encrypt the configuration file using the provided utility, load it in the support ticket and you will receive provisioned validation devices by our Hardware Secure Module (HSM) equipped factories.

Benefits of Using the TrustFLEX ATECC608B with AWS IoT Core

  • Create secure authentication to IoT devices powered by AWS IoT Core
  • Benefit from the scalability of AWS IoT Core (including China)
  • Leverage AWS Just-In-Time-Registration and Use Your Own Certificate
  • Provide a unique, trusted, protected and managed device identity
  • Pre-configured with most popular use cases
  • Turn-key code examples available for each use case 
  • Leverage Microchip’s secure provisioning service
  • Simplify logistics of shipping private keys and reduce manufacturing costs
  • Microcontroller-agnostic implementation
  • JIL rated “high” secure key storage
  • Protection against known tamper, side-channel attacks

TrustFLEX ATECC608B-TFLXTLS Use Cases

Each of the device slots are pre-configured to offer the following use cases:
  • Custom Certificate Authentication
  • Token Authentication
  • Secure Boot (with key attestation)
  • Over-the-Air (OTA) Verification
  • Firmware Intellectual Property (IP) Protection
  • Message Encryption
  • Key Rotation
  • I/O Protection Key
  • Host Accessory Authentication

Visit the ATECC608B-TFLXTLS product page to learn more about the device’s features.

Are You Interested in AWS IoT Greengrass Hardware Security Integration?


Find out how to develop an IoT Greengrass Hardware Security Integration solution using the ATECC608B secure element.

Trust Platform Devices


Development Tools


Learning


Title Description
How to Use Microsoft® Azure® RTOS and the ATECC608 TrustFLEX Secure Element In this blog you can read about how to implement a secure boot and Transport Layer Security (TLS) mutual authentication for your Internet of Things (IoT) device.
How Transport Layer Security (TLS) and Secure Elements Work In this blog you can learn about the importance of TLS and the embedded security pillars as encryption is weak without robust secure key storage to protect the private key.
Asymmetric Authentication Use Case Example The purpose of authentication is to prevent cloning and counterfeiting and to ensure that an object is genuine and authorized to connect to a product. In this use case example, find out how to authenticate an object, such as an accessory, peripheral, battery or cartridge, that is typically removable and replaceable by the consumer.
Secure Firmware Download Use Case Example In this use case example, you will see a demonstration of the authentication of a firmware update. The example uses asymmetric cryptography to establish a chain of trust to validate the update.
Securing Cloud-Connected Devices with Google Cloud IoT and Microchip This blog article written by Google discusses how the ATECC608B secure element strengthens authentication between IoT Core and IoT hardware.
Symmetric Authentication Use Case Example The purpose of authentication is to prevent cloning and counterfeiting and to ensure that an object is genuine and authorized to connect to a product. In this use case example, find out how to authenticate an object, such as an accessory, peripheral, battery or cartridge, that is typically removable and replaceable by the consumer.
Symmetric Authentication with a Non-Secure MCU Use Case Example In this use case example, you will learn how to authenticate an object using one-way symmetric authentication, which avoids the need for an Internet connection and white (or black) list. A white list is a lookup table for identifying approved units and a blacklist is a lookup table for identifying non-approved units.
Zero Touch Secure Provisioning Kit for AWS IoT - End-to-End Security with AWS Cloud This user's guide provides a detailed walkthrough of provisioning the Zero Touch Secure Provisioning Kit to connect and communicate with the Amazon Web Services (AWS) IoT service.

General Questions:

Q: How can I get started with the Trust Platform?
A:
 Use the “Let Us Guide You to the Right Option” on the Trust Platform page, which will help you take the first step. You will find additional information about getting started with Trust&GOTrustFLEX and TrustCUSTOM on their pages.

Q: I am a distribution partner. How do I enroll in the Trust Platform program?
A:
 Contact your local Microchip sales office to request assistance with joining the program.

Trust&GO Questions:

Q: Do I need to contact Microchip to provision my Trust&GO secure element?

A: No. When you buy the device, it is already provisioned with keys and certificates specific to the use case you have selected that are locked inside the device. Trust&GO cannot be altered and is intended to be used as is.

Q: Where can I obtain the public keys and certificates for my Trust&GO device?
A: Log into your customer account at the ecommerce website where you purchased the device after device shipment, and you should be able to download a manifest file containing all the necessary public keys and certificates. Contact the vendor if you have any trouble finding this file.

TrustFLEX Questions:

Q: Do I need to contact Microchip to provision my TrustFLEX secure elements?  
A:
 Yes. When you buy the device, it comes pre-configured with your selected use case(s). By default, the TrustFLEX device also come with keys and generic certificates for thumbprint authentication that are overwritable internally if you have not already locked them using the lock bit. While the configuration cannot be altered, the default credentials can be changed if you have not already locked them. If you decide to use the default credentials, you will have to lock them after receiving the device. If you don’t want to use the default credentials, you can replace them with yours and then lock them. After you have made your decision, create the secret packet exchange, encrypt it and upload it into a support ticket on Microchip’s technical support portal. We will provision your devices and ship them according to your instructions.

Q: Where can I obtain the public keys and certificates for my TrustFLEX device when I use the default credentials?
A:
 Log into your customer account at the ecommerce website where you purchased the device after device shipment, and you should be able to download a manifest file containing all the necessary public keys and certificates. Contact the vendor if you have any trouble finding this file. WARNING: If you have overwritten the default credentials in your device, the manifest file will no longer be compatible with the device’s new credentials.

TrustCUSTOM Questions:

Q: Do I need to contact Microchip to provision my TrustCUSTOM secure element?
A:
 Yes. When you buy the device, it will be blank. You will need to use the TrustCUSTOM configurator, which is available under Non-Disclosure Agreement (NDA) to define the configuration, create the secret packet exchange, encrypt it and upload it into a support ticket on Microchip’s technical support portal. We will provision your devices and ship them according to your instructions.

Q: Where can I obtain the secret packet exchange for my TrustCUSTOM device?
A:
 This utility is only available through a Non-Disclosure Agreement (NDA). Contact your local Microchip sales office or distributor to request it.

Q: Where can I get the full data sheet for my TrustCUSTOM device?
A:
 This document is only available through a Non-Discloser Agreement (NDA). Contact your local Microchip sales office or distributor to request it.

Credentials: Identity verification tools or methods that include X.509 certificates, generic certificates for thumbprint authentication, keys and data packets

Customization: The action of creating a unique device/system through its configuration and set of secrets

Firmware Verification: When a key and cryptographic operation are used to verify a signed image on a device at boot up or during run time

IP Protection: When a key and a cryptographic operation are used to verify signed (or hashed) firmware that is considered Intellectual Property (IP) of a product

Key(s): A set of binary numbers that is used to trigger a cryptographic algorithm that implements asymmetric or symmetric encryption

Over-the-Air (OTA) Verification: When a key and a cryptographic operation are used to verify a signed image that has been loaded into a connected device by a push notification from a cloud service

PKI: Public Key Infrastructure

Provisioning: The action of generating a credential into an embedded storage area

Birth Certificate: An X.509 certificate not issued by a certificate authority company that is used for authentication to the cloud

 

Use cases:

Custom Certificate Authentication: Use the default generic certificates for thumbprint authentication already inside the TrustFLEX device or overwrite them with your own certificates.

Token Authentication: Leverage a private key to perform an Elliptic Curve Digital Signature Algorithm (ECDSA) sign operation on a token that will be verified by its corresponding public key somewhere else in the network.

Secure Boot (with key attestation): Perform an ECDSA verification at boot using a public key corresponding to a private key used to sign the code which the system will boot from. The public key becomes highly sensitive as it will allow a system to boot.

Over-the-Air (OTA) Verification: Perform an ECDSA verification after an update using a public key corresponding to a private key used to sign the code the system will be updated with. The public key becomes highly sensitive as it will allow a system to be updated with a new code that needs to be trusted.

Firmware Intellectual Property (IP) Protection: Perform a verification during the system runtime using a key corresponding the one used to sign the code the system will run on. The verification key becomes highly sensitive as it will allow a system to run on a genuine code image.

Message Encryption: Provides the capability to encrypt a very small packet of data using the integrated hardware Advanced Encryption Standard (AES) engine.

Key Rotation: Provides the capability to rotate private keys within the secure boundaries of the secure element.

I/O Protection Key: Provides the capability to uniquely pair the MCU and the secure element.

Host Accessory Authentication: Provides the capability to create an ecosystem control strategy by having a main host authenticate its peripherals using a basic PKI architecture.