FPGA designers choose VectorBlox Accelerator for its key capabilities that include:
VectorBlox 3.0 compression reduces memory usage and data movement by supporting both structured and unstructured compression techniques. Structured compression targets regular data such as weights, activations and feature maps with known layouts, enabling deterministic compression and low‑overhead decompression in hardware. Unstructured compression supports sparse and irregular data patterns by storing only nonzero values and their indices. Together, these approaches allow larger models and higher resolution data to operate within fixed memory and bandwidth constraints on edge and embedded systems.
Discover five key enhancements in the VectorBlox™ Accelerator SDK 3.0, and see how the latest release helps developers deploy AI more efficiently on PolarFire® FPGAs and SoCs.
Follow these steps to begin using the VectorBlox Accelerator SDK:
Install the VectorBlox™ SDK and review the Programmer’s Guide.
Convert your CNN using one of the tutorial scripts found in our tutorials section. If you have successfully converted your CNN without any errors, proceed to the next step; otherwise, reach out to us.
The PolarFire SoC FPGA is supported by the VectorBlox SDK. To get started quickly, purchase the PolarFire SoC Video Kit and visit the video kit demo on GitHub.
Install the Libero SoC Design Suite to view or rebuild the referene design components
Click on the “Request Free License” link below to generate the free Libero SoC Design Suite Silver and CoreVectorBlox licenses. Then merge the two licenses*.
*Refer to section 7.3 of the Libero software quick-start guide to learn how to merge these licenses.
Key features of the CoreVectorBlox IP include:
The VectorBlox SDK includes framework-dependent quantization tools that convert FP32 models to INT8, along with compilation tools that generate binaries and weights. These assets are stored in nonvolatile memory, typically Serial Peripheral Interface (SPI) Flash, and loaded into Double Data Rate (DDR) memory when the SoC FPGA powers on.
The PolarFire SoC Video Kit is designed to evaluate the VectorBlox SDK. It includes a preconfigured reference design with a MIPI CSI-2®-based camera interface, an HDMI® input, Image Signal Processing (ISP) pipeline, the VectorBlox SDK AI engine and an HDMI output for displaying results.
In this webinar, you'll discover how VectorBlox™ 3.1 streamlines Convolutional Neural Network (CNN) compression, enables direct mapping of sparsity into FPGA hardware and supports the deployment of power-efficient AI inference solutions for intelligent edge applications across industries, such as industrial automation and aerospace.
We will also feature our partner, Atlas Engineering, showcasing their VectorBlox-powered turnkey solutions that help customers deploy mission-critical autonomous systems efficiently and reliably.
Seamlessly integrating high-speed sensor data with NVIDIA's AI-driven Holoscan platform, our Ethernet sensor bridge for NVIDIA Holoscan is an essential solution for industries that use AI. This bridge enables advanced imaging capabilities in medical, industrial, automotive and other sectors.
In healthcare, NVIDIA Holoscan enhances medical imaging and robotic surgery by processing sensor data quickly for accurate diagnostics and interventions. The low-latency communication of the Ethernet sensor bridge allows cloud AI computations closer to data sources, improving system responsiveness and efficiency.
Live Chat