===================================================================================================================== Linux v1.01.33 Driver Release Notes for SMSC LAN95XX Family USB 2.0 to Ethernet Controller and USB Hub with Ethernet ===================================================================================================================== Contents: 1. Platforms and OS versions supported 2. Device support 3. Driver structure and file description 4. Building and installing the driver 5. Release history 6. Testing 7. Known issues 8. Driver initialization parameter 9. Debugging 1. Platforms and kernel versions supported ------------------------------------------ - x86/x64 bit PC - kernel up to 3.10.x 2. Device support ----------------- This release supports: -LAN9500 -LAN9512/LAN9513/LAN9514 -LAN9500A -LAN9530/LAN9730/LAN89530 3. Driver structure and file description ---------------------------------------- This driver is comprised of two modules: smscusbnet.ko: Usbnet interface layer (derived from usbnet.ko in Linux kernel) smsc9500.ko: lan9500 hardware specific module. Source files: smscusbnet.h - usbnet header file smscusbnet.c - usbnet source file smsc9500.h - lan9500 hardware specific header file smsc9500.c - lan9500 hardware specific source file ioctl_9500.h - ioctl header file definitions cmd9500.c - application for useful debugging. version.h - Driver version number header file. 4. Building and installing the driver ------------------------------------- The following instructions work fine for a PC build environment, embedded platforms may need slight build modifications, consult your platform documentation. a. Obtain the kernel source tree for the platform in use and build it. b. build using "./build", the smscusbnet.ko & smsc9500.ko modules are created. c. load both modules in the following sequence: insmod smscusbnet.ko insmod smsc9500.ko d. Plug in the lan9500 device into the USB port. e. Configure the ethernet interface eth in the usual way for an ethernet device. 5. Release history ------------------- V1.01.33 (01/22/2014) - Added explicit net_carrier_off() in bind() - Changed Rx and Tx queue size V1.01.32 (12/04/2013) - Fixed some code analysis tool errors V1.01.31 (10/21/2013) - Fixed issue of unable to go to suspend on Tegra platform V1.01.30 (08/12/2013) - Fixed issue in reading empty eeprom through ethtool V1.01.29 (07/10/2013) - Fixed compilation error on 3.10.x V1.01.28 (04/02/2012) - Reduced EEPROM write time with cmd9500 tool WRITE_FILE_TO_EEPROM option V1.01.27 (11/30/2012) - Handling ETIME error (OHCI) - Fix crash on PPC platform V1.01.26 (10/12/2012) - Resolved compilation issues with 3.6.x kernel V1.01.25 (07/30/2012) - Added MII_BUSY flag when accessing phy registers - Fixed ethtool link reporting V1.01.24 (05/11/2012) - Added support for kernel up to 3.3.0 V1.01.23 (02/24/2012) - Added more ethtool options V1.01.22 (01/16/2012) - Fixed bug for validate MAC address V1.01.21 (09/26/2011) - Fixed bug for link polling timer V1.01.20 (06/10/2011) - Fixed link issue - Change not to submit BulkIn request when the link goes down V1.01.19 (06/09/2011) - Added support PME for EepromLess operation - Fixed bug for report link status V1.01.18 (03/23/2011) - Fixed bug for flow Control - Added support for LAN9530/LAN9730/LAN89530 v1.01.17 (03/07/2011) - Added module parameter to clone or copy tx skb. Forcing copy tx skb will provide alignment required by some host controller. v1.01.16 (01/21/2011) - Changed not to check eeprom size during the initialization time. v1.01.15 (01/19/2011) - Fixed error checking while reading from internal RAM v1.01.14 (01/18/2011) - Fixed attach/detach bug. v1.01.13 (12/17/2010) - Added support for kernel up to 2.6.37 v1.01.12 (09/15/2010) - Fix bug: unable to set mac address (kernel <29) - Fix Ethtool speed and auto-negotiation options v1.01.11 (09/03/2010) - Fix for EEPROM write through ethtool v1.01.10 (05/04/2010) - EDPD settings for LAN9500A - Automdix fix v1.01.09 (04/29/2010) - Support of changing mac address through ifconfig command - Fixed ethtool speed setting options - Fixed auto_mdix disable mode options v1.01.08 (04/20/2010) - Use GFP_DMA flag while allocating memory for usb control transfers - Added reset_resume - Reading PHY_BSR twice while link check - Build issues with kernels up to 2.6.34 - ethtool -k gets correct status for rx_csum - changed smartdetach to netdetach v1.01.07 (03/10/2010) - Software workaround for tx checksum offload (1 or 2 byte udp payload) hw bug. v1.01.06 (01/26/2010) - Added .ndo support for kernels 2.6.29 and up. v1.01.03 (10/09/2009) - Fixed a configuration problem. If kernel configuration CONFIG_USB_SUSPEND is disabled and autosuspend is enabled, previous version won't transfer any packets. v1.01.02 (6/23/2009) - Fixed the problem that previous version didn't support kernel without power management enabled. - Removed some false EEPROM warning messages. - Added smartdetach support when kernel version is less than 2.6.18 for LAN9500A. - Fixed a minor memory issue. v1.01.01 (4/30/2009) - Fixed bug that linkdown suspend didn't work on LAN9500A. - Fixed unresponsive problem sometimes when smartdetach is enabled. - Added new commands WRITE_FILE_TO_EEPROM, READ_EEPROM_TO_FILE, VERIFY_EEPROM_WITH_FILE in the utility cmd9500. v1.01.00 (4/16/2009) - Enable PHY energy detection before entering dynamic suspend. Therefore, driver gets chance to switch suspend state when link changes. v1.00.10 (4/06/2009) - Support dynamic suspend for LAN9500 and LAN9500A. - Support smart detach for LAN9500A. - Update statistics counters for LAN9500A. - Add EEPROMless support for LAN9500 and LAN9512. - Add LAN9500A alternative LED configuration. v1.00.09 (3/27/2009) - Add support for separate LEDs for link activity and link status. - Add support that device will suspend when link is down. v1.00.08 (3/20/2009) - Add support for LAN9512/9514. - Add support for LAN9500A. - Fix a bug related to ethtool command "ethtool -s ethX autoneg off". v1.00.07 (10/20/2008) - Add GET_ERRORs command to cmd9500 to retrieve internal USB error counters. - Enable autosuspend function (only for kernet 2.6.19 and higher) NOTE: in order to use this feature it needs to be enabled in the kernel as well. For this type "echo auto > /sys/bus/usb/devices/5-7/power/level", (where ../5-7/.. is bus number of the device) from the shell. - Expand error recovery for any kind of USB pipe errors. - Fixed compile wanrnings for x64 kernel builds. v1.00.06 (internal release) - Support x64 (64 bit PC) kernels builds. - Add error recovery for TXE. - Add cmd9500 application to access lan9500 registers and perform other task of interest (mostly for debugging) v1.00.05 (internal release) - Add support for automdix overide strap. 6. Testing ---------- This is an engineering release. 7. Known Issues ---------------------------- - When using operational_mode=1 (which is not the not the driver's default), we have observed that the device could become unusable if a USB hot swap is performed while stressing active traffic (i.e. ping flood) is ongoing. We have determined this to be caused by a bug in the linux kernel v2.6.25 and higher related to handling of periodic transactions. While the kernel patch currently being proposed (http://marc.info/?t=121837892200003&r=1&w=2) solved that particular problem it introduced others, so it is not a good solution. Once a stable kernel patch for this issue is available this problem should be resolved. - On some Linux distributions such as Centos, "pcscd" daemon keeps accessing LAN9500/LAN9500A/LAN9512 device for some reasons, which prevents LAN9500 device from entering suspend state. To solve this problem, You can disable it by typing "chkconfig pcscd stop". - To enable autosuspend automatically, add following lines into the file /etc/udev/rules.d/50-udev.rules ACTION==”add”, SUBSYSTEM==”usb_device”, SYSFS{idVendor}==”0424”, SYSFS{idProduct}=="9500",RUN+=”/bin/sh -c 'echo auto > /sys/$DEVPATH/device/power/level'” ACTION==”add”, SUBSYSTEM==”usb_device”, SYSFS{idVendor}==”0424”, SYSFS{idProduct}=="9e00",RUN+=”/bin/sh -c 'echo auto > /sys/$DEVPATH/device/power/level'” ACTION==”add”, SUBSYSTEM==”usb_device”, SYSFS{idVendor}==”0424”, SYSFS{idProduct}=="ec00",RUN+=”/bin/sh -c 'echo auto > /sys/$DEVPATH/device/power/level'” You may have to replace vendor id and product id with your own customized IDs. - When netdetach is enabled, you have to setup network configuration script to bring up network interface automatically. Suppose smsc9500 Ethernet interface is eth0. Add following lines into /etc/sysconfig/network-scripts/ifcfg-eth0. DEVICE=eth0 ONBOOT=no BOOTPROTO=static IPADDR=192.168.1.40 8. Driver Initialization parameters ----------------------------------- There are several possible parameters for each driver module a. smscusbnet.ko - operational_mode: 0: low_latency mode. Device uses bulk in pipe continuous reader for ethernet rx. This is the default mode. 1: low power mode. Device uses the interrupt pipe to detect ethernet rx, only then submits bulk in's to read rx data. Once no rx data available stops bulk in submissions. - rx_queue_size: controls the size of the rx queue default is 60 - tx_queue_size: controls the size of the tx queue default is 60 - tx_hold_on_completion default is 1 (enabled). If set the driver will not submit a new bulk out urb until all previously ones submitted complete b. smsc9500.ko - link_mode: A bit wise field that specifies any combination of 4 or fewer link speeds 0x01: 10HD 0x02: 10FD 0x04: 100HD 0x08: 100FD 0x10: Symmetrical Pause 0x20: Asymmetrical Pause 0x40: Auto Negotiate - auto_mdix: allows overide to strap in order to control phy's automdix behavior 0: Disable AMDIX, Straight Cable 1: Disable AMDIX, CrossOver Cable 2: Enable AMDIX 3: Controlled by Strap - mac_addr_hi16 & mac_addr_lo32: allow Ethernet Mac address overide. - scather_gather: enabled kernel S/G support (needed for tx_Csum) - tx_Csum: Default to 0. Set to 1 to enable hw tx checksum support - rx_Csum: Default to 0. Set to 1 to enable hw rx checksum support - phy_addr: Default to 1 and using internal phy. Set to appropriate values if connecting an external phy. - TurboMode: receive mode 0: One receive packet per bulk in transaction 1: Multiple receive packet per bulk in transaction - debug_mode: controls amount of debug verbosity (see debugging below) - linkdownsuspend: 0: Disabled. 1: Enabled with normal power savings (recommended for maximum compatibility) 2: Enabled with maximum power savings. - LinkActLedCfg: if true, enable hardware driven LED configuration on LAN9500A. Only applies to LAN9500A. - LinkLedOnGpio: Selects the GPIO number (in the range 0 to 10) use for link status indication. If this parameter is not specified, the LED handling is the original hardware default for combined link/activity pin. - LinkLedBufType: if enabled (will be only if LinkLedOnGpio is used), set GPIO port buffer type as open-drain. Otherwise, it is push/pull. - LinkLedPolarity: if enabled (will be only if LinkLedOnGpio is used), GPIO output will be low active. Otherwise, will be high active. - dynamicsuspend: if enabled, suspend device automatically if no traffic for 3 seconds, then waking up device if any Tx/Rx traffic. - netdetach: if enabled, detach device from USB bus if link is down, then re- attaching device to USB bus if link is back. 9. Debugging ------------ a. You can use the debug_mode insmod parameter to control printk verbosity of this driver. See DBG_xxx #defines in smsc9500.h for details. b. The cmd9500.c provides several useful commands that can facilitate runtime debugging by allowing register manipulations and/or giving access to internal driver data. See it's usage page DisplayUsage() for details.