**************************** LAN7500 Windows CE 5.0&6.0 Console Utility V0.2 **************************** The LAN7500 application provides a console utility to program the EEPROM of LAN7500 device. 1. Supported OS =========================== Windows CE 5.0&6.0 2. Starting LAN7500 Utility =========================== To use the CE7500eep utility, double click the CE7500eep icon or run it at the command line. 3. Using LAN7500 Utility ======================== When run, the following options are available: 1. program EEPROM 2. program & Verify EEPROM 3. Read EEPROM Q. Exit Selecting option 1 or 2 will write the EEPROM. For these options, the user must provide the EEPROM contents in a binary file located in the \Windows\ directory. The file name must be 7500.bin. Selecting option 3, “Read EEPROM”, will read the EEPROM contents to a binary file, 7500.bin, located in the \Windows\ directory. Selecting Q, will exit the application. 4. Known Issues =============== None