Smart
Flame Detector Application Demonstration on PIC32CM LE00 Curiosity Pro
Evaluation Kit
Description:
This application demonstrates detection of flame using Flame Click,
and if the flame has been detected, it alerts through the Microchip
Bluetooth Data (MDB App) and on the OLED Display.
Further, the flame detection data is also logged with the help of SD
Card (Along RTC Timestamp). Additionally, user can reset the RTC
timestamp by pressing SW0 switch.
Modules/Technology Used:
Hardware Used:
This project has been verified to work with the following versions of
software/development tools: - Refer Project
Manifest present in harmony-manifest-success.yml under the project
folder firmware/src/config/pic32cm_le00_cpro
Because Microchip
regularly update tools, occasionally issue(s) could be discovered while
using the newer versions of the tools. If the project doesn’t seem to
work and version incompatibility is suspected, It is recommended to
double-check and use the same versions that the project was tested with.
To download original version of MPLAB® Harmony v3 packages,
refer to the document How
to Use the MPLAB® Harmony v3 Project Manifest Feature
Hardware Setup:
- Connect the two mikroBUS Xplained Pro boards to the
Extension Header EXT1 (J601) and Extension
Header EXT3 (J603) of the PIC32CM LE00 Curiosity Pro
Evaluation Kit, as shown below:

- Connect the I/O1 Xplained Pro Extension Kit to the
Extension Header EXT2 (J602) of the PIC32CM
LE00 Curiosity Pro Evaluation Kit and plug the SD Card into the
microSD Card Connector of the I/O1 Xplained Pro
Extension Kit, as shown below:

- Mount the FLAME CLICK on the mikroBUS
Xplained Pro which has been connected to the Extension
Header EXT3 (J603), and mount the RNBD451 Add On
Board on the mikroBUS Xplained Pro which has
been connected to the Extension Header EXT1 (J601) of
the PIC32CM LE00 Curiosity Pro Evaluation Kit, as shown
below:

- Mount the OLED C CLICK on the mikroBUS
Header Connector of the PIC32CM LE00 Curiosity Pro
Evaluation Kit, as shown below:

- The overall hardware set-up of the demo is as shown below:

- Using a Type-A USB-Micro-B USB cable, connect the
Type-A Male to your PC, and Micro-B USB
Male to your Micro-B DEBUG USB port (J300) of
the PIC32CM LE00 Curiosity Pro Evaluation Kit to power
it, and to program and debug the application.
RNBD Setup:
Follow these instructions to setup the RNBD before running the demo:
- Connect the RNBD451 Add On Board as a standalone to
your host microcontroller or PC, using a USB Type-C
Cable. To power this standalone module, change the
Power Supply Selection (J7) jumper - Open a serial
terminal application (such as Tera Term) on your PC - To enter command
mode, send the charaters $$$ as instruction - Set the
baud rate to 9600 using SB command and the instruction is
SB,03 - Enable pin UART Transparent mode and Bluetooth
Status LED using SR command and the instruction is
SR,0101 - Reboot the module to save the changes using R
command with the instruction R,1 - Reposition the
Power Supply Selection (J2) jumper to power from the
host board and mount the RNBD451 Add On Board on the
hardware setup
Programming hex file:
The pre-built hex file can be programmed by following the below steps:
### Steps to program the hex file: - Open MPLAB® X IDE - Close all
existing projects in IDE, if any project is opened. - Go to
File -> Import ->
Hex/ELF File - In the “Import Image File”
window, Step 1 - Create Prebuilt Project,
click the”Browse” button to select the prebuilt hex
file. - Select Device has “PIC32CM5164LE00100” - Ensure
the proper tool is selected under “Hardware Tool” -
Click on “Next” button - In the “Import Image
File” window, Step 2 - Select Project Name and Folder, select
appropriate project name and folder - Click on “Finish”
button - In MPLAB® X IDE, click on “Make and Program
Device” Button. The device gets programmed in sometime. -
Follow the steps in the Running the Demo
section below ## Programming/Debugging Application Project: - Open the
project
(pic32cm_le00_cpro_smart_smoke_detector/firmware/pic32cm_le00_cpro.X)
in MPLAB® X IDE - Ensure “PIC32CM LE00 Curiosity Pro”
is selected as hardware tool to program/debug the application - Build
the code and program the device by clicking on the “Make and
Program Device” button in MPLAB® X IDE tool bar - Once
programming is complete and successful, perform a power cycle of
the board. - Note: A power cycle is mandatory
because only upon power-on-reset (POR), does the SPI_SCK pin which is
shared between OLED and RNBD reinstates as expected. Else, the OLED may
not start-up properly. - Follow the steps in Running the demo section below ## Running
the Demo: - Perform Hardware Setup and Programming/Debugging
Application Project steps mentioned above, if not done already. -
For demonstration, the Flame Click is used to detect
the flame. Shining a flashlight on the flame click sensor should be good
enough to trigger it, for demo purposes. - If the flame has been
detected, the Flame Labeled LED(Flame Presence LED
Indicator) in the Flame Click will glow. - The OLED
display shows the ADC result values of the Flame sensor periodically as
shown here:
- The SD Card log the
flame detection message along with the Timestamp (RTC). - To get the
fire alarm detection in the mobile app, please proceed the following
steps: - Install the Microchip Bluetooth Data Android App in your
Android Smartphone using the
MicrochipBluetoothData_Smartsmoke.apk file under the
project folder Android_App. Alternatively, Click
here to download it. - Enable and allow Bluetooth and location from
Smartphone settings - Open the “Microchip Bluetooth Data
(MBD)” android app from your smartphone and tap on “BLE
UART” icon on the dashboard. If prompted, allow the application
to turn on Bluetooth, as shown:

- Click on flame detector option from the list, as shown:

- Now, scan for RNBD451 Bluetooth device under the Device window and
connect it. The RNBD device should appear as RNBD451_XXXX
(deviceId) in the list of Bluetooth devices. After, click on
it. Note, for your setup, the deviceId may vary

- Select the “Text Mode option”, as shown:

- Then, the GUI of the mobile app, displays the fire detection data, as
shown:

- Reference Material:
- This application demo builds and works out of box by following the
instructions above in Running the Demo
section. If you need to enhance/customize this application demo, you
need to use the MPLAB® Harmony v3 Software framework. Refer links below
to setup and build your applications using MPLAB® Harmony v3.
- v1.7.0 Initial Release of the demo.