Getting Started Application on PIC32CK GC01 Curiosity Ultra Development Board

Download


Description

This application demonstrates an LED toggle (LED0 toggles when the switch SW0 is pressed) on a timeout basis and print the LED toggling rate on the serial terminal. The periodicity of the timeout will change from 500 milliseconds to one second, two seconds, four seconds, and back to 500 milliseconds every time you press the switch SW0 on the PIC32CK GC01 Curiosity Ultra Development Board.

The demo application has an extended functionality to read and print the current room temperature periodically when the extension header (EXT1) is plugged with the I/O1 Xplained Pro Extension Kit. The temperature reading is displayed on a serial console periodically.

Modules/Technology Used:

Hardware Used:

Software/Tools Used:

This project has been verified to work with the following versions of software tools:

Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/pic32ck_gc01_cult
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version. Alternatively, Click Here.
- Any Serial Terminal application like Tera Term terminal application.

Because Microchip regularly update tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project doesn’t seem to work and version incompatibility is suspected, It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature

Setup 1:

Setup 2:

Programming hex file:

The pre-built hex file can be programmed by following the below steps

Steps to program the hex file

Programming/Debugging Application Project:

Note: This application is programmed using the PKOB4 tool pack v1.14.1168. If the user sees issues with programming, please install this tool pack version and use it accordingly.

Running the Demo:

Comments:

Revision: